Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on November 16, 2007: 071116/tn2

The Real-Time OS--HI1000/4--for the H8SX and H8S MCU Families Revised to V.1.05 Release 00


The real-time OS--HI1000/4--for the H8SX and H8S MCU families has been revised from V.1.04 Release 00 to V.1.05 Release 00.

1. Product and Versions to Be Updated
Product: HI1000/4
Versions: V1.0.05,
V1.0.06,
V.1.01 Release 00,
V.1.02 Release 00,
V.1.03 Release 00,
V.1.04 Release 00
2. Description of Revision
   The following two problems have been fixed, which are explained in 
   RENESAS TOOL NEWS Document No. 071116/tn1, "Notes on Using the Real-
   Time OS--HI1000/4--for the H8SX and H8S MCU Families," published in
   this series of news:
    (1) With issuing the chg_pri service call
    (2) With issuing the ter_tsk service call
   For details, see the above news at
     http://tool-support.renesas.com/eng/toolnews/071116/tn1.htm
   (available on and after December 5, 2007).

3. How to Update Your Product and Purchase the Revised One
3.1 Free-of-Charge Update
    Free-of-charge online update is available. If you are using the product 
    to be updated, download the installer of the product's update program 
    from the Web site at 
       http://www.renesas.com/itron_download
    This site will be opened from December 5 on.

3.2 First Ordering
    If you place an order for the product, please supply the following 
    items of information to your local Renesas Technology sales office 
    or distributor (for the price of the product, also contact them):
Product Type: HI1000/4
Type Name: R0R41600TRW01w
Version No.: V.1.05
Release No.: Release 00
Host OS: Windows XP, Windows Me, Windows 98, Windows 2000, Windows NT 4.0
 NOTICE:
       Lower-case letter w at the end of the type name denotes the type 
       of license. It shall be replaced with any one of the following 
       numerals and upper-case letters:
1:
Evaluation license; a real-time OS can be installed only to
one host computer.
5:
Evaluation license; a real-time OS can be installed up to
5 host computers.
A:
Evaluation license; a real-time OS can be installed up to
10 host computers.
K:
Mass-production license; a real-time OS can be embedded up to a total of 1,000 productions of product model(s) with the source code not disclosed.
U:
Mass-production license; a real-time OS can be embedded up to unlimited productions of product model(s) with the source code not disclosed.
Z:
Mass-production license; a real-time OS can be embedded up to unlimited productions of product model(s) with the source code disclosed.
 Example: 
         For mass-production license up to a total of 1,000 productions 
         with the source code not disclosed, letter w shall be replaced 
         with letter K; that is, the type name is R0R41600TRW01K.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal