Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on November 16, 2007: 071116/tn5

The Converter Board--R0E5212L4CFG00-- for the R8C/2K and R8C/2L MCU Groups Released


We have released the converter board--R0E5212L4CFG00--for the R8C/2K and R8C/2L groups, R8C/Tiny series of MCUs. This board connects user systems designed with above-mentioned MCUs (encapsulated in the 32-pin 0.8-mm-pitch LQFP package, PLQP0032GB-A) to the emulator or compact emulator for the R8C/Tiny series.

1. Features
   The R0E5212L4CFG00 is a converter board for the user system designed 
   with any member of the R8C/2K and R8C/2L MCU groups (encapsulated in the 
   32-pin 0.8-mm-pitch LQFP package, PLQP0032GB-A) and is used to connect 
   the user system to the emulation probe--R0E521000EPB00--or the compact 
   emulator--R0E521000CPE00--for the R8C/Tiny series to emulate the system.
   For details of the specifications of the board, see its user's manual 
   from here.(This is 4-page, 619-KB PDF file.)
   
   
   Note that to emulate systems designed with MCUs in the R8C/2K and R8C/2L 
   groups using the R0E521000EPB00 emulation probe or R0E521000CPE00 compact 
   emulator, you need the MCU files containing information specific to 
   those MCUs.
   For how to get these MCU files, see Section 3 of RENESAS TOOL NEWS 
   Document No. 071116/tn4, "MCUs Added to the Support Lines of the Emulation 
   Probe--R0E521000EPB00--and the Compact Emulator--R0E521000CPE00--
   for the R8C/Tiny MCU Series," published on November 16, 2007, at
      http://tool-support.renesas.com/eng/toolnews/071116/tn4.htm#sect_3
   (available on and after November 20, 2007).

   For information on the R0E521000EPB00 emulation probe and R0E521000CPE00 
   compact emulator, see their datasheets on the Web sites listed below.
    R0E521000EPB00: http://www.renesas.com/pc7501/r0e521000epb00
    R0E521000CPE00: http://www.renesas.com/r0e521000cpe00

2. The Contents of the Product Package
   (1) A converter board--R0E5212L4CFG00--for the R8C/2K and R8C/2L 
       MCU groups
   (2) A socket at a probe end--YQPACK032SA (manufactured by Tokyo 
       Eletech Corp.)
   (3) A socket for mounting the target MCU--NQPACK032SA 
       (manufactured by Tokyo Eletech Corp.)
   (4) Four guide pins--YQ-GUIDE (manufactured by Tokyo Eletech Corp.)
   (5) A user's manual

3. Ordering Information
   If you place an order for the product, please supply the following 
   items of information to your local Renesas Technology sales office 
   or distributor (for the price of the product, also contact them):

3.1 Converter Board Only
        Product Type: R0E5212L4CFG00
        Type Name:    As above

3.2 Combination of Converter Board with Emulation Probe or Compact Emulator
    The converter board can be supplied in combination with the 
    R0E521000EPB00 emulation probe or the R0E521000CPE00 compact emulator.
	
    (1) Combination with the emulation probe
        Product Type: R0E5212L4EPB00
        Type Name:    As above
		
    (2) Combination with the compact emulator
        Product Type: R0E5212L4CPE00
        Type Name:    As above



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal