|
|
 |
RENESAS TOOL NEWS on November 16, 2007: 071116/tn6
| Flash Development Toolkit Revised
to V.3.07 Release 04 |
Flash Development Toolkit has been revised from V.3.07 Release 03 to
V.3.07 Release 04. This tool kit is used for programming flash memory of the
MCUs in the SuperH RISC engine, M16C, H8SX, H8S, H8, and 740 families.
1. Descriptions of Revision
1.1 Supported MCUs Increased
The following MCUs have been added to the support line:
| In the H8S family |
H8S/2280BF, H8S/2280RBF, H8S/2602F, H8S/2604F, H8S/2607F,
H8S/2609F |
| In the H8 family |
H8/38002F |
The above MCUs are programmable via the RS-232C port or the HS0008EAUF1H
adaptor board for on-board programming.
1.2 Problem Fixed with Programming QzROM-version MCUs in the 740 Family
The problem with programming the internal ROM of QzROM-version MCUs
in the 7545, 7546, 7547, 7548, and 7549 groups, 740 family has been
fixed.
For details, see RENESAS TOOL NEWS Document No. 070916/tn5, published
on September 16, 2007, at
http://tool-support.renesas.com/eng/toolnews/070916/tn5.htm
2. How to Update Your Product
Free-of-charge online update is available. Download the installer of
the latest program from the Web site at
http://www.renesas.com/fdt_download
and execute it. This site will be opened on and after November 20.
Note that you are not able to update your toolkit to V.3.07 Release 04
using AutoUpdate Utility.
3. Notices
(1) This revision aims at making the MCUs supported by Flash Development
Toolkit V.4.00 Release 02 be also supported by the V.3 product.
That is, it is not the revision from V.4.00 Release 02.
(2) If AutoUpdate Utility is executed in the PC where Flash Development
Toolkit V.3.07 Release 03 resides, the evaluation version of the
V.4 product will be installed.
(3) We plan no further revision of the V.3 product. So this is the last
time to add MCUs to its support line.
(4) The V.3 product cannot be used in combination with the E8a emulator.
|
 |