|
|
 |
RENESAS TOOL NEWS on December 1, 2007: 071201/tn1
| A Note on Using the C Compiler Packages for the M16C Family of MCUs |
Please take note of the problem described below in using the C compiler
packages for the M16C family of MCUs.
1. Products and Versions Concerned
C compiler package for the M32C series* (M3T-NC308WA)
V.5.00 Release 1 through V.5.40 Release 00
C compiler package for the M16C series** (M3T-NC30WA)
V.5.10 Release 1 through V.5.40 Release 00A
* The M32C series is the generic name of the M32C/80, and M16C/80
series.
** The M16C series is the generic name of the M16C/60, /30, /20, /10,
/Tiny and R8C/Tiny series.
2. Description
If a write to and a read from a bit field are made before and after
calling a function respectively, the value of the bit field may become
incorrect.
3. Conditions
This problem may occur if the following conditions are all satisfied:
(1) Any of the optimizing options -O[1-5],-OR, and -OS is selected.
(2) A bit field is used whose storage class is auto.
(3) The bit field in (2) is not qualified to be volatile.
(4) A write is made to the bit field in (2).
(5) The program performs either of the following after the write in (4):
(a) A call is made to the function that takes the address of the
structure containing the bit field in (2) as its argument.
(b) A call is made to a function immediately after the address of
the structure containing the bit field in (2) is assigned to
another variable.
(6) The value of the bit field in (2) is changed within either of the
functions in (5)-(a) and (5)-(b).
(7) The bit field in (2) is accessed after a call is made to either
of the functions in (5)-(a) and (5)-(b)
Example:
------------------------------------------------------------------------
struct tag{ // Conditions (2) and (3)
unsigned char b0:1;
unsigned char b1:1;
unsigned char b2:1;
unsigned char b3:1;
unsigned char b4:1;
unsigned char b5:1;
};
main()
{
struct tag bit2;
bit2.b1 = 1; // Condition (4)
func(&bit); // Condition (5)-(a)
if(bit2.b1==1) // Condition (7)
sub();
}
------------------------------------------------------------------------
4. Workaround
Place a dummy asm function between a write to the bit field and a call
to the function involved.
------------------------------------------------------------------------
. . . . . . . . . . . . . . . . . . . .
main()
{
struct tag bit2;
bit2.b1 = 1;
asm(); // Place asm function
func(&bit);
. . . . . . . . . . . . . . . . . . . .
------------------------------------------------------------------------
5. Schedule of Fixing the Problem
This problem has already been resolved in the following versions of the
products concerned:
- C compiler package for the M32C series (M3T-NC308WA) V.5.41 Release 00
- C compiler package for the M16C series (M3T-NC30WA) V.5.42 Release 00
So use these or later versions.
|
 |