Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 1, 2007: 071201/tn2

A Note on Using the Real-Time OS
--HI1000/4 V.1.05 Release 00--
for the H8SX and H8S Families of MCUs


Please take note of the following problem in using the real-time OS-- HI1000/4 V.1.05 Release 00--for the H8SX and H8S families of MCUs:
  • With selecting the product's release note among the Start menu of Windows (R)


1. Product and Version Concerned
    HI1000/4 V.1.05 Release 00

2. Description
   When you select the product's release note among the Start menu of 
   Windows (R), the Missing Shortcut dialog box may open, 
   and you are not able to open the release note.

3. Condition
   This problem occurs if you select the release note among the Start menu 
   of Windows (R) for the first time after installing the product.

4. Solution
   Press the Browse button in the Missing Shortcut dialog box; 
   then select HI1000_4_10500_REL_071101_E_.pdf in the \Manuals\english 
   folder, which you will find under the folder where you have installed 
   HI1000/4.
   If you open the release note once such a way, thereafter you can open 
   the release note by selecting it among the Start menu of Windows (R).



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal