Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 1, 2007: 071201/tn4

Corrections to a Catalog Published on October 2007


We notify corrections to the following catalogs, which were published in October 2007:
  1. Renesas Quick Reference Guide to Semiconductor Devices
    Document No. REJ02A0003-0800 (printed and PDF editions)

  2. Renesas USB Device
    Document No. REJ01B0005-0501 (PDF edition)
The corrections described below can be seen on the Web site at
http://www.renesas.com/tool_catalog
This site will be opened from December 20 on.

A. Corrections to "Renesas Quick Reference Guide to Semiconductor Devices" 
   Document No. REJ02A0003-0800
   1. Page 86, body of the table; first row from the top in the Full-spec
      emulator column (in the SH7136 and SH7137 Group row)
      Read (E200F) R0E0200F1EMU00 *13 *20 for (E200F) R0E0200F1EMU00 *13

   2. Ibid., notes under the table
      Add the following note after *19:
      *20. The E200F emulator can't evaluate I2C by using the system 
           configuration with the Evaluation chip unit. In order to evaluate 
           I2C, please install the H-UDI port connector (36-pin type) on 
           the user system and use it with the system configuration without 
           the Evaluation chip unit.

   3. Page 97, "Adaptor board" column (second from the right) of the top 
      table
      Through the column exist three R0E000080AKCE00s. Read R0E00008AKCE00 
      for each of them: R0E000080AKCE00

   4. Page 98, "Adaptor board" column (second from the right) of the table
      Through the column exist three R0E000080AKCE00s. Corrections are the 
      same as in Item 3 above.

   5. Page 99, "Adaptor board" column (second from the right) of the table
      Through the column exist three R0E000080AKCE00s. Corrections are the 
      same as in Item 3 above.

   6. Page 100, "Adaptor board" column (second from the right) of the top 
      table
      Through the column exists an R0E000080AKCE00. Correction is the same 
      as in Item 3 above.

B. Correction to "Renesas USB Device"
   Document No. REJ01B0005-0501
   1. Page 32, "Programmer (Flash)" column (extreme right) of Development 
      Tools for the H8SX, H8S Family's table
      Through the column exist six R0E000080AKCE00s. Corrections are the 
      same as in Item 3 of Section A above.

C. Related Information
      We notified a correction to this catalog in the following RENESAS TOOL NEWS.





© 2003-2010 Renesas Technology Corp., All rights reserved. Web Site Usage Conditions| Privacy| Sitemap