1. Product and Versions Concerned
High-performance Embedded Workshop V.4.01.00 through V.4.03.00
High-performance Embedded Workshop is bundled with the compilers and
other software products that it manages.
To check for the version number of your High-performance Embedded
Workshop, open the Help menu and select the About High-performance
Embedded Workshop command.
2. Problem
Each time the debugger accesses any file to debug, the Open dialog
box may open, and the path of the file be asked in projects
created by using Makefile.
3. Condition
This problem occurs if you are using any of the following debuggers:
- M32C PC7501 emulator debugger
- M32C PC4701 emulator debugger
- M32C compact emulator debugger
- M32C simulator debugger
- M32C FoUSB/UART debugger
- M16C R8C PC7501 emulator debugger
- M16C PC4701 emulator debugger
- M16C R8C compact emulator debugger
- M16C R8C FoUSB/UART debugger
- M16C R8C simulator debugger
- 740 PC4701 emulator debugger
- 740 compact emulator debugger
- 740 simulator debugger
- H8/300H Tiny compact emulator debugger
4. Solution
This problem has been fixed in High-performance Embedded Workshop
V.4.04.00, which was released in this December 16.
For details of High-performance Embedded Workshop V.4.04.00, see
RENESAS TOOL NEWS Document No. 071216/tn5, published on December 16,
2007, in this series of news.