|
|
 |
RENESAS TOOL NEWS on January 16, 2008: 080116/tn1
| A Note on Using the C/C++ Compiler Package
for the M32R Family of MCUs |
Please take note of the following problem in using the C/C++ compiler
package--M3T-CC32R--for the M32R family of MCUs:
- With using an assignment expression whose left term is of a shorter
data type than the right term and after which is placed an expression
that is equivalent to the right term of the assignment expression
1. Product and Versions Concerned
C/C++ compiler package--M3T-CC32R--for the M32R family
V.3.20 Release 1 through V.5.00 Release 00
2. Description
Consider the case where an assignment expression whose left term is
of a shorter data type than the right term exists, and after it is
placed another expression that contains an expression equivalent to
the right term of the assignment expression.
When the second expression is evaluated, such a value is used that is
obtained by casting the operation result of the right term of the
assignment expression to the shorter data type; not the above operation
result itself.
3. Conditions
This problem may occur if the following conditions are all satisfied:
(1) The optimizing option used in compilation meets either (a) or (b)
shown below.
(a) Option -O, -O2, -O3, -O6, or -O7 is used.
(b) Option -Ospace or -Otime is used with -O0, -O1, -O4, and -O5
not used.
(2) An expression exists which contains more than one variable of an
integral type and whose operation result is also of an integral type.
The expression can contain only one variable of an integral type.[h1]
(3) An assignment expression exists in which the operation result of
the expression in (2) is assigned to an auto variable of a shorter
integral type than the operation result in (2).
(4) An expression equivalent to the expression in (2) is used as
a part of another expression evaluated after the assignment
expression in (3).
(5) Between the assignment in (3) and the use of an expression in (4)
exists no possibility of changing the values of any variables
contained in the expression in (2).
(6) The auto variable in (3) is saved on the stack; not on a register.
(7) The operation result of the expression in (2) is saved on
a register. This is valid when the expression contains only one
variable.
NOTICE:
Whether the objects in Conditions (6) and (7) are saved on the stack
or a register depends on your compiler and is not determined by the
source code. It should be checked using the code generated after
compilation.
Example:
In the operation of expression val_ulong >> 8 below is used the value
of val_ulong after assigned to val_uchar. So the operation result of
this expression becomes incorrect. However, this problem may not arise
depending on the descriptions of the program lines that are omitted
below.
-------------------------------------------------------------------------
unsigned long func_ulong(unsigned short);
void func(void)
{
unsigned long val_ulong;
unsigned char val_uchar;
unsigned int val_another;
unsigned short val_ushort;
/*
. . . . . . . . . . . . . . . . . . . . . . .
*/
val_ulong = func_ulong(val_ushort);
val_uchar = val_ulong; /* Conditions (2) and (3) */
val_another = val_ulong >> 8; /* Conditions (4) and (5) */
/*
. . . . . . . . . . . . . . . . . . . . . . .
*/
}
-------------------------------------------------------------------------
4. Workarounds
Avoid this problem in either of the following ways:
(1) Suppress the optimization in Level 2.
If you are using option -O, -O2, -O3, -O6, or -O7, replace it
with -O0, -O1, -O4, or -O5.
If you are using -Ospace or -Otime, use -O0, -O1, -O4, or -O5
at the same time.
(2) Exchange the expressions in Conditions (3) and (4) in their order.
Example modified:
--------------------------------------------------------------------
unsigned long func_ulong(unsigned short);
void func(void)
{
. . . . . . . . . . . . . . . . . . . . . . .
val_ulong = func_ulong(val_ushort);
val_another = val_ulong >> 8; /* Conditions (4) and (5) */
val_uchar = val_ulong; /* Conditions (2) and (3) */
. . . . . . . . . . . . . . . . . . . . . . .
}
--------------------------------------------------------------------
5. Schedule of Fixing the Problem
This problem has already been fixed in the V.5.01 Release 00 package.
So use the latest version of the package. Note that the package V.4.30
Release 00 or earlier cannot be updated to the latest version. If this
is the case, please purchase the latest version.
|
 |