Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on January 18, 2008: 080118/tn1

High-performance Embedded Workshop Revised to V.4.04.01


High-performance Embedded Workshop (IDE) has been revised from V.4.04.00 to V.4.04.01.

1. Product and Versions to Be Updated
   High-performance Embedded Workshop V.3.00.00 through V.4.04.00

   High-performance Embedded Workshop is bundled with the compilers and 
   other software products that it manages.
   To check for the version number of your High-performance Embedded 
   Workshop, open the Help menu and select the About High-performance 
   Embedded Workshop command.

2. Description of Revision
   The following problem has been fixed:
     When your High-performance Embedded Workshop updated to V.4.04.00 is 
     launched, it may be terminated abnormally.
   For details see RENESAS TOOL NEWS Document No. 080110/tn1, published on 
   January 10, 2008, at 
     http://tool-support.renesas.com/eng/toolnews/080110/tn1.htm

3. How to Update Your Product
   Free-of-charge online update is available. Use either of the following 
   ways to update yours:
   (1) Download the update program* of the product from the Web site shown 
       below and execute it.
         http://www.renesas.com/hew_download
       This Web site will be opened from January 21 on.
   (2) Use AutoUpdate Utility** to download the update program of 
       the product; then execute it.
       This service will be provided on and after January 22.
   Note that the above two ways of updating do not update any components 
   except High-performance Embedded Workshop; that is, no C compilers, 
   emulator debuggers, and others updated.

   NOTES:
      *Three types of update program are available. Use any of them 
       depending on the IDE you are using. They are as follows:
       (a) Full update program
           The components of High-performance Embedded Workshop to which 
           changes have been made in and after V.3.00.00 are updated; 
           that is, V.3.00.00 and later can be updated.
       (b) Differential update program from V.4.04.00
           The components of High-performance Embedded Workshop to which 
           changes have been made in and after V.4.04.00 are updated; 
           that is, V.4.04.00 can be updated.
       (c) Differential update program from V.4.03.00
           The components of High-performance Embedded Workshop to which 
           changes have been made in and after V.4.03.00 are updated; 
           that is, V.4.03.00 and later can be updated.

     **When you are using AutoUpdate Utility whose version falls in 
       a range from V.1.00.00 to V.1.03.00, update it to V.1.04.00; then 
       update your High-performance Embedded Workshop to V.4.04.01.
       AutoUpdate Utility was revised to V.1.04.00 on July 1, 2007.
       For details see RENESAS TOOL NEWS Document No. 070701/tn1, 
       published on July 1, 2007, at
          http://tool-support.renesas.com/eng/toolnews/070701/tn1.htm



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal