|
|
 |
RENESAS TOOL NEWS on February 1, 2008: 080201/tn2
| The Emulator Software Product for the E200F Emulator
R0E0200F1EMU00 Revised to V.2.05 Release 00 |
We have revised the emulator software product for the E200F emulator
R0E0200F1EMU00 from V.2.04 Release 00 to V.2.05 Release 00.
The emulator and software product emulate systems designed with SH-2
and SH2A CPU-cored MCUs, belonging to the SuperH RISC engine family.
1. Descriptions of Revision
1.1 The following devices have been added to the support line:
MCU Series Devices
------------------------------------------------------
SH7280 Devices in SH7286 group
SH7137 Devices in SH7136 and SH7137 groups
SH7147 SH7142 devices (R5F71424xxxxxxx), SH7147 group
1.2 The following problem, encountered in the SH7206 device, has been fixed:
When the external bus trace unit is connected with the evaluation chip
unit, the signal levels of buses obtained as Strobe_signals for external
bus tracing are incorrectly displayed as follows, as well as bus names:
- The name and signal level of /RASU and those of /RASL are swapped.
- The name and signal level of /CASU and those of /CASL are swapped.
If the external trace bus unit is not connected with the evaluation
chip unit, this problem does not occur.
2. How to Update Your Product
Free-of-charge online update is available. Use AutoUpdate Utility;
otherwise use the following procedure:
(1) Download the update program of the product (a ZIP file) from
the Web site at
http://www.renesas.com/e200f_download
This site will be opened from February 5 on.
(2) Decompress the downloaded ZIP file to obtain the installer program
HewInstMan.exe and execute it.
3. Notice
If the installer program is executed in the system where
High-performance Embedded Workshop V.4.02.00 or earlier resides,
it will be upgraded to V.4.03.00.
|
 |