Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on February 1, 2008: 080201/tn3

Brand-New Full-Featured Emulator
E100 Released


We have released a brand-new full-featured emulator--E100--for Renesas's 8- to 32-bit MCUs.

1. Outline
   The E100 emulator is designed for common use with most of Renesas's 
   8- to 32-bit MCUs to be developed from now on except those belonging to 
   the SuperH and M32R families and R32C series. It is used in combination 
   with the MCU unit and converter board* for each of the supported MCUs; 
   that is, if you want to replace a target MCU with another, all necessary 
   to do is to replace the MCU unit and converter board with those for 
   another.

   In comparison with our previous full-featured emulators, the E100 comes 
   with the following improved features: the capability of recording trace 
   data of 4 megacycles maximum, that of making full use of tracing results 
   by enhancing filtering functions, and so on.
   In addition, the newly introduced features such as real-time profiling 
   and detection of un-initialized items provide you with expanded 
   debugging environments.
   For further information on the E100, see its datasheets in the Web site at 
           http://www.renesas.com/e100

   NOTE:
    *The MCU unit and converter board for each supported MCU are optional.
     (Those for the M16C/60 and H8S/Tiny series are under development.)

2. Contents of the Product Package
   (1) An E100 emulator
   (2) An AC adaptor for 100- to 240-V, 50/60-Hz mains
   (3) A power cable
   (4) A USB-interface cable
   (5) A setup guide

   E100 emulator debugger is included with each MCU unit for the E100.
   Its latest version will become downloadable from our Web site as MCU 
   units go on the market.

3. Ordering Information
   When you place an order for the product, supply the following items of 
   information to your local Renesas Technology sales office or distributor:
Product Type: E100
Type Name: R0E001000EMU00
 
   For the price of the product, contact the above sales office or 
   distributor.

4. Note on the WS Product of the E100 Emulator
   The WS product of the E100 emulator does not differ from the commercial 
   version of the E100 in any functionality, so please use the WS product 
   as it is if you are using it.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal