Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on February 5, 2008: 080205/tn2

A Note on Using E8a Emulator Software - With performing single-step execution in 740 E8a Emulator Debugger -


Please take note of the following problem in using the emulator software for the E8a on-chip debugging emulator:
  • With performing single-step execution in 740 E8a Emulator Debugger (when MCUs of the 740 family targeted)


1. Product and Versions Concerned
   E8a Emulator Software
   V.1.00 Release 00 and V.1.00 Release 00A

2. Description
   If the line containing the BBC or BBS instruction of the 740 MCU 
   family is single-stepped in the 740 E8a Emulator Debugger included in 
   the product concerned, the program may not halt at the next instruction 
   to be executed but continue running (single-step execution not ended).

3. Conditions
   This problem may occur if the following conditions are all satisfied:
   (1) The 740 E8a Emulator Debugger included in the product concerned 
       is running.
   (2) In the program exists the BBC or BBS instruction used in the ZERO 
       PAGE BIT RELATIVE addressing mode, and a bit stored in memory 
       addresses 80h to FFh is used as a branch condition.
   (3) The instruction in (2) above is single-stepped.

   Example:
   -------------------------------------------------------------------------
   BBC 0, 80h, 0E123h  ; Bit 0 in address 80h used as a branch condition
   BBS 0, FFh, 0E123h  ; Bit 0 in address FFh used as a branch condition
   -------------------------------------------------------------------------

4. Workaround
   If step execution not ended, press the Stop button of High-performance 
   Embedded Workshop.
   NOTICE:
   If the Stop button pressed, the program may not halt at the instruction 
   to be executed next to the BBC or BBS instruction, but halt at the address 
   whose instructions were executed at that time.

5. Schedule of Fixing the Problem
   This problem has been resolved in E8a Emulator Software V.1.01 Release 00,
   which will be released on and after February 6. So use the latest version.
   For details of V.1.01 Release 00, see RENESAS TOOL NEWS Document No. 
   080201/tn4, published on the same date, on the Web page at
      http://tool-support.renesas.com/eng/toolnews/080205/tn4.htm
   This site will be opened from February 5 on.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal