|
|
 |
RENESAS TOOL NEWS on March 1, 2008: 080301/tn1
| A Note on Using High-performance Embedded Workshop |
Please take note of the following problem in using High-performance Embedded
Workshop:
- With the IDE neglecting build error messages when a real-time OS is
being used
1. Description
Suppose you are making the build of a project that uses a real-time OS.
Even if the "Create Jump table" utility in the real-time OS outputs
any error or warning messages, High-performance Embedded Workshop does
not interpret these as errors or warnings. So these messages, when
displayed in the Output window, do not come with error or warning marks
and are not included in the error and warning count provided after the
build is complete.
2. Conditions
This problem occurs if any one of the following combinations of a
compiler package and a real-time OS is used on High-performance
Embedded Workshop:
(1) The C compiler package for the R32C/100 series V.1.01 Release 00 and
the real-time OS for the R32C series (M3T-MR100/4) V.1.00 Release 00
(2) Either of the C compiler packages for the M32C series (M3T-NC308WA)
V.5.41 Release 00 and V.5.41 Release 01, and
Any of the real-time OSes for the M32C series M3T-MR308 V.1.10
Release 1 through V.1.20 Release 1B or either of M3T-MR308/4
V.4.00 Release 00 and V.4.00 Release 01
(3) Any of the C compiler packages for the M16C series (M3T-NC30WA)
V.5.42 Release 00 through V.5.43 Release 00, and
Any of the real-time OSes for the M16C series M3T-MR30 V.3.10
Release 1 through V.3.30 Release 2 or M3T-MR30/4 V.4.00 Release 00
3. How to Check Error and Warning Messages
The error and warning messages of the "Create Jump table" utility are
displayed just behind the first line of Linker Phase messages in the
Build tab in the Output window.
So scroll the window to find top of Linker Phase messages and read them
to judge if they are error and warning messages.
4. Schedule of Fixing the Problem
This problem is due to modules of the High-performance Embedded
Workshop included in each of the compiler packages involved.
So we are fixing this problem in the next release of those compilers
by including the problem-fixed modules with their packages.
|
 |