Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on March 1, 2008: 080301/tn4

The Debugging MCU Board for the SH7147 MCU Series (HS7147EDB01H) Released


We have released the debugging MCU board HS7147EDB01H, which is used for debugging systems designed with either of the two MCUs of the SH7147 series, SH7147 or SH7142, in combination with the E10A-USB emulator (HS0005KCU01H and HS0005KCU02H, these emulators are used for the SuperH RISC engine, H8S, and H8SX families of MCUs).

1. Outline of Product
   Because the SH7147 and SH7142 MCUs (in the SH7147 series) are not provided 
   with the user debugging interface function (H-UDI), systems designed with 
   either of them cannot be debugged using the E10A-USB emulator.
   However, the debugging MCU board HS7147EDB01H, in combination with the 
   above E10A-USB emulator, enables you to configure an economical 
   debugging environment: a simple in-circuit emulator.

   For details of the product, visit the Debugging MCU Board page from 
   the Web site (E10A-USBs' site) at
          http://www.renesas.com/e10a_usb
   Information on the HS7147EDB01H board is being released on this page 
   from March 5 on.

2. Contents of Product Package
   (1) An debugging MCU board:   HS7147EDB01H
   (2) An IC socket:             NQPACK100SD-ND
                                   (mfd. by Tokyo Eletech Corp.)
   (3) A cover of the IC socket: HQPACK100SD
                                   (mfd. by Tokyo Eletech Corp.)

3. How to Purchase Product
   The debugging MCU board is available as the single board only or the 
   combination of the board and the E10A-USB emulator HS0005KCU02H*.
   When you place an order for either of them, supply its product type and 
   type name listed below to your local Renesas Technology sales office 
   or distributor.
Product Type
Type Name
Debugging MCU board only HS7147EDB01H
Combination of Debugging MCU board and E10A-USB emulator HS0005KCU02H HS7147EDB01H-E1
   For the prices of them, contact the above sales office or distributor.

4. Notice
   When you use the debugging MCU board with the E10A-USB emulator, 
   it is necessary that E10A-USB Emulator Software V.2.11 Release 00 
   or later be installed in your PC. For details of the V.2.11 Release 00 
   software, see RENESAS TOOL NEWS Document No. 080301/tn3 on the Web page at
     http://tool-support.renesas.com/eng/toolnews/080301/tn3.htm.


© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal