1. Descriptions of Revision
1.1 Features
(1) The debugger is usable with the compact emulator for the 455A MCU
group, M3455AT2-CPE.
For information on the M3455AT2-CPE, see RENESAS TOOL NEWS
document No. 080301/tn5 on the Web page at
http://tool-support.renesas.com/eng/toolnews/080301/tn5.htm.
(2) The following data files of the 455A group have been included:
| MCU |
Data File |
| M3455AG8 |
M3455AG8.DAT |
| M3455AGC |
M3455AGC.DAT |
1.2 Problem Fixed
The following problem has been fixed: If the ROM data of the area
including addresses 0x3F80 to 0x3FFF is uploaded, an error arises
in MCUs whose maximum ROM address is 0x3FFF.
The MCUs involved in this problem are as follows:
- M34571GD
- M34583MD
- M34584MD
2. How to Update Your Product
Free-of-charge online update is available as described below.
(1) Download the update program, an EXE file, of the product from the
Web site at
http://www.renesas.com/m3455at2_cpe_download
(This site will be opened from this March 21 on).
(2) Execute the downloaded file (pd45mv122r00_e.exe).