Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on March 16, 2008: 080316/tn1

A Note on Using High-performance Embedded Workshop


Please take note of the following problem in using High-performance Embedded Workshop:
  • With transferring load modules from PC to debugging platform


1. Product and Versions Concerned
   High-performance Embedded Workshop
     V.4.02.00 through V.4.04.01

2. Description
   When you open the Debug menu, select Download, and then select 
   All Download Modules or pathname of load module file to transfer 
   load module(s) from PC to debugging platform, application errors 
   may arise.

3. Conditions
   This problem occurs if the following conditions are all satisfied 
   when you open the Debug menu, select Download, and then select 
   All Download Modules or pathname of load module file to transfer 
   load module(s):
    (1) The "Run to main function on reset" check box in the Debug tab
        of the Options dialog box has been checked.
    (2) The "Use Disassembly source-mode as primary debug view" 
        check box in the same tab in (1) above has also been checked.
    (3) The Disassembly window is not open.

4. Workarounds
   To transfer load module from PC to debugging platform, double-click the
   load module file displayed in the Projects tab in the Workspace 
   window, or use the pop-up menu that appears when you right-click the 
   icon of the "Download modules" folder displayed in the above tab.

5. Schedule of Fixing the Problem
   We plan to fix this problem in the next release of the product.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal