Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on April 1, 2008: 080401/tn3

MCUs Added to the Support Lines of the Emulation Probe --R0E521000EPB00--and the Compact Emulator--R0E521000CPE00-- for the R8C/Tiny Series of MCUs


The MCUs coming with 32-KB ROM of the R8C/28 and R8C/29 groups have become supported by the emulation probe--R0E521000EPB00--and the compact emulator --R0E521000CPE00--for the R8C/Tiny series of MCUs.

1. Descriptions
   The R0E521000EPB00 emulation probe and the R0E521000EPB00 compact 
   emulator have started supporting the MCUs coming with 32-KB ROM (the J 
   and K versions) of the R8C/28 and R8C/29 groups.
   To emulate systems designed with these MCUs, their respective MCU files 
   and release notes are necessary. An MCU file contains information 
   specific to the corresponding MCU, and a release note does information 
   on debugging and evaluating MCU-based target systems.
   For how to obtain MCU files and release notes, see Section 2. 

   To connect the emulation probe or compact emulator with the user system, 
   use the converter board--R0E521174CSJ00--for the 20-pin 0.65-mm-pitch 
   LSSOP package. For details of this converter board, see its user's manual 
   on the Web page at
   http://documentation.renesas.com/eng/products/tool/rej10j0847_r0e521174csj00_u.pdf
   (a 228-KB PDF file of 4 pages). 
       The above URL is that of our global site (in English).

2. How to Obtain MCU Files and Release Notes
   We supply you with the MCU files for the MCUs with 32-KB ROM of the 
   R8C/28 and R8C/29 groups and the release notes for these MCUs in which 
   information on debugging and evaluating target systems are described 
   We prepare the release note and the installer of the MCU files for 
   the R0E521000EPB00 and the R0E521000CPE00 each, as listed below.
   Download the release note and the installer of the MCU files you want 
   from the Web page at 
     http://tool-support.renesas.com/eng/toolnews/download/r8c26_29.htm
   (available on and after March 7, 2008).
   Then execute the downloaded installer to add the newly-supported MCUs' 
   MCU files to your emulator debugger.
   
   (1) For emulation probe R0E521000EPB00
        Installer:    MCU_Files_install_epb_R8C_26-29.exe
        Release note: rej10j0894_r0e521000epb00_s.pdf
		
   (2) For compact emulator R0E521000CPE00
        Installer:    MCU_Files_install_cpe_R8C_26-29.exe
        Release note: rej10j0863_r0e521000cpe00_s.pdf

   NOTICE:
     Be sure to read through the release note for your system before 
     using the R0E521000EPB00 and/or R0E521000CPE00.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal