Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on April 4, 2008: 080404/tn1

Flash Development Toolkit Revised to
V.4.01 Release 01


We have revised Flash Development Toolkit from V.4.01 Release 00 to V.4.01 Release 01. This tool kit is used for programming flash memory of the MCUs in the SuperH RISC engine, M16C, H8SX, H8S, H8, and 740 families.

1. Descriptions of Revision
1.1 Supported MCUs Increased
    The following MCUs have been added to the support line:
    (1) In the H8SX family
          H8SX/1725F
		  
    (2) In the H8S family
          H8S/2112F, H8S/2153F, H8S/2164F, H8S/2462F, and H8S/2472F
		  
    (3) In the H8 family
          H8/36022F, H8/36092F, H8/38502F, H8/38504F,
          H8/38522F, H8/38524F, H8/38534F, and H8/38537F
		  
    The MCUs in (1), (2), and (3) above are programmable via the 
    RS-232C port, the HS0008EAUF1H board (an on-board programming 
    adaptor board for flash MCUs), or the E8a emulator.
	
    (4) In the M16C family
          R5F3640M (M16C/64 group, M16C/60 series)
            This is programmable via the RS-232C port or the E8a emulator. 
          R5F21286 and R5F21296 (R8C/Tiny series)
            These are programmable via the E8a emulator.

1.2 Supported Interfaces Increased
    (1) The E8a emulator can be used for programming the following MCUs 
        as well as RS-232C and HS0008EAUF1H:
          H8S/2265F and H8S/2266F (H8S family)
          H8/36012F, H8/38327F, H8/38347F, H8/38427F, 
          and H8/38447F (H8 family)
		  
    (2) The RS-232C port can be used for programming the following MCUs 
        as well as the E8a and E8 emulators:
          R5F212A7, R5F212A8, R5F212B7, R5F212B8, R5F212C7, R5F212C8, 
          R5F212D7, and R5F212D8 (R8C/Tiny series, M16C family)

2. How to Update Your Product
   Free-of-charge online update is available. Download the installer of 
   the latest program from the Web site at 
     http://www.renesas.com/fdt_download
   and execute it. This site will be opened from April 7 on.
       The above URL is that of our global site (in English).

   If you are using the V.4.00 Release 00 or later product, AutoUpdate 
   Utility is available from April 8 on.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal