|
|
 |
RENESAS TOOL NEWS on June 16, 2008: 080616/tn8
| A Note on Using the Debuggers for the R8C/Tiny MCU Series |
Please take note of the following problem in using the debuggers for the
R8C/Tiny MCU series:
- With using the IO files for the R8C/2A, /2B, /2C, and /2D groups
included in the debuggers for the R8C/Tiny MCU Series
1. Products and Versions Concerned
M16C R8C PC7501 Emulator Debugger V.1.03 Release 00
M16C R8C Compact Emulator Debugger V.1.03 Release 00
M16C R8C FoUSB/UART Debugger V.1.03 Release 00
M16C R8C Simulator Debugger V.1.03 Release 00
E8a Emulator Software V.1.00 Release 00 through V.1.01 Release 00
E8 Emulator Software V.2.09 Release 02 through V.2.11 Release 00
2. Descriptions
Incorrect descriptions are found in the IO files for the R8C/2A, /2B,
/2C, and /2D MCU groups included in the above products.
Due to these incorrect descriptions, the name of the mode register for
UART2 is expressed as UART0 in the IO windows on each debugger.
3. Workaround
Use the problem-fixed IO files. The procedures of how to obtain them
and substitute them for the previous files are as follows:
(1) Download the problem-fixed and compressed IO file R8C2xIO.zip
(38 KB) from the Web page at
http://tool-support.renesas.com/eng/toolnews/080616/R8C2xIO.zip
This page will be opened on and after July 4.
(2) Decompress the downloaded file.
(3) With the decompressed file, overwrite the file with the same name
under the folder where High-performance Embedded Workshop resides.
For instance, if the IDE has been installed in the folder
C:\Program Files\Renesas\Hew
the IO file for each debugger will be found in the folder following
the debugger's name listed below.
- M16C R8C PC7501 Emulator Debugger
C:\Program Files\Renesas\Hew\Tools\Renesas\DebugComp\Platform\PDTarget\PD30F\IO Files
- M16C R8C Compact Emulator Debugger
C:\Program Files\Renesas\Hew\Tools\Renesas\DebugComp\Platform\PDTarget\PD30MF\IO Files
- M16C R8C FoUSB/UART Debugger
C:\Program Files\Renesas\Hew\Tools\Renesas\DebugComp\Platform\PDTarget\KD30\IO Files
- M16C R8C Simulator Debugger
C:\Program Files\Renesas\Hew\Tools\Renesas\DebugComp\Platform\PDTarget\PD30SIM\IO Files
- E8a Emulator Software
C:\Program Files\Renesas\Hew\Tools\Renesas\DebugComp\platform\E8a\E8aR8C\IOFiles
- E8 Emulator Software
C:\Program Files\Renesas\Hew\Tools\Renesas\DebugComp\Platform\E8\E8R8C\IOFiles
4. Schedule of Fixing the Problem
We plan to fix this problem in the next release of those debuggers.
|
 |