Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on July 1, 2008: 080701/tn2

A Note on Using the C Compiler Package
for the R32C Series, M16C MCU Family V.1.01 Release 00


Please take note of the following problem in using the C compiler package for the R32C series, M16C MCU family V.1.01 Release 00:
  • With setting options in the load module converter


1. Description
   When the High-performance Embedded Workshop included in the product 
   concerned is running, none of the addresses ranging from 0x0F000000 
   through 0xFFFFFFFF can be typed into the address parameters of the -A, 
   -E, and -F options text box, Lmc tab, Toolchain dialog box.
   To open the Toolchain dialog box, open the Build menu and select 
   the Renesas R32C/100 Standard Toolchain command; then select the
   Lmc tab.

   Descriptions of Options:
     Option -A: Enters the address range of the machine language outputted 
                to the generated file.
     Option -E: Enters the beginning address of user program.
     Option -F: Enters arbitrary values for the addresses that have not 
                been outputted in the specified absolute module file.

2. Workaround
   Open the Toolchain dialog box, select the Lmc tab, Categories drop-down 
   list, and Others. Then type the user-specified option with the parameter 
   into the Load Module Converter Options text box as a character string of 
   command line options.
      Example: 
         When outputting data value 0x0 to the generated file in an address 
         range of 0x0F000000 through 0xFFFFFFFF, type as follows:
             -A 0:0F000000:0FFFFFFFF

3. Schedule of Fixing the Problem
   We plan to fix this problem in the next release of the product.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal