|
|
 |
RENESAS TOOL NEWS on July 16, 2008: 080716/tn4
| A Note on Using the Licensed Tools for Adding
Device Groups to E10A-USB Emulators' Support Lines |
Please take note of the problem described below in using the licensed tools
for adding device groups to E10A-USB emulators' support lines.
E10A-USB emulators are used for the SuperH RISC engine, H8S, and H8SX MCU
families.
1. Products and Versions Concerned
The following licensed tools for adding device groups to E10A-USB
emulators' support lines are concerned. They can only be used for
the E10A-USB emulators HS0005KCU01H and HS0005KCU02H.
(1) Licensed tool for the SH-4A device group:
HS7780KCU01SR V.2.00 Release 00 and V.3.00 Release 00
(2) Licensed tool for the SH-4 device group:
HS7751KCU01SR V.2.00 Release 00 and V.3.00 Release 00
(3) Licensed tool for the SH-3 device group:
HS7729KCU01SR V.2.00 Release 00 and V.3.00 Release 00
(4) Licensed tool for the SH-2A device group:
HS7206KCU01SR V.2.00 Release 00 and V.3.00 Release 00
(5) Licensed tool for the SH-2 device group:
HS7047KCU01SR V.2.00 Release 00 and V.3.00 Release 00
(6) Licensed tool for the SH-Mobile device group:
HS7290KCU01SR V.2.00 Release 00 and V.3.00 Release 00
(7) Licensed tool for the New_SH-Mobile device group:
HS7318KCU01SR V.2.00 Release 00 and V.3.00 Release 00
(8) Licensed tool for the H8S device group:
HS2339KCU01SR V.2.00 Release 00 and V.3.00 Release 00
(9) Licensed tool for the H8SX device group:
HS1527KCU01SR V.2.00 Release 00 and V.3.00 Release 00
For details of these licensed tools from here.
The above URL is that of our global site (in English).
2. Description
If any of the above license tools is installed to the host computer,
the association of High-performance Embedded Workshop with workspace
files (.hws files) is lost. So double-clicking the name of any workspace
file will not invoke High-performance Embedded Workshop.
3. Solution
Download the update program to High-performance Embedded Workshop
V.4.04.01 (the latest version) from the Web site shown below and
reinstall the latest version of the High-performance Embedded Workshop
(See NOTE.)
http://www.renesas.com/hew_download
The above URL is that of our global site (in English).
NOTE:
The following two types of update program are available. Use either
of them:
(a) Full-update program
(b) Differential-update program
Or, use AutoUpdate Utility to update yours.
For details see RENESAS TOOL NEWS at
http://tool-support.renesas.com/eng/toolnews/080118/tn1.htm
The above URL is that of our global site (in English).
After the solution above has been executed, the problem occurs again
when any of the product concerned is installed.
In that case, implement the solution again.
4. Schedule of Fixing the Problem
We plan to fix this problem in the next release of the license tools.
|
 |