Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on Aug. 1, 2008: 080801/tn2

Hardware Tools Released
in the Last Half of July 2008


We released the hardware tools described below in the last half of July 2008.

1. Hardware Tools for the R8C/Tiny Series, M16C Family
   (1) For the R8C/32A group
       A converter Board--R0E53032ACSJC0--for the 20-pin 0.65-mm-pitch 
       LSSOP: 
         Connects the MCU unit R0E521300MCU00 (under development), which is 
         used for the E100 emulator, to the foot pattern for the members of 
         the R8C/32A group encapsulated in the 20-pin 0.65-mm-pitch LSSOP 
         package. (See NOTE below.)

       For details of the board, see its user's manual on the Web page at
http://documentation.renesas.com/eng/products/tool/rej10j1878_r0e53032acsjc0_u.pdf

   (2) For the R8C/33A group
       A converter Board--R0E53033ACFG90--for the 32-pin 0.8-mm pitch LQFP:
         Connects the MCU unit R0E521300MCU00 (under development), which is 
         used for the E100 emulator, to the foot pattern for the members of 
         the R8C/33A group encapsulated in the 32-pin 0.8-mm-pitch LQFP 
         package. (See NOTE below.)

       For details of the board, see its user's manual on the Web page at
http://documentation.renesas.com/eng/products/tool/rej10j1872_r0e53033acfg90_u.pdf

   (3) For the R8C/36E, R8C/36F, R8C/36G, and R8C/36H groups
       Converter Board--R0E53036ACFK40--for the 64-pin 0.5-mm pitch LQFP:
         Connects the MCU unit R0E521300MCU00 (under development), which is 
         used for the E100 emulator, to the foot pattern for the members of 
         the R8C/36E, R8C/36F, R8C/36G, and R8C/36H groups encapsulated in 
         the 64-pin 0.5-mm-pitch LQFP package. (See NOTE below.)

       For details of the board, see its user's manual on the Web page at
http://documentation.renesas.com/eng/products/tool/rej10j1873_r0e53036acfk40_u.pdf

    NOTE:
      The MCU unit R0E521300MCU00 is under development. For the MCUs 
      supported by this unit, see its datasheets on the Web site from here.
      It is that of our global site (in English). 

2. Ordering Information
   The product types are as follows the type names are the same as those:
     R0E53032ACSJC0 (Converter board for the R8C/32A group) 
     R0E53033ACFG90 (Converter board for the R8C/33A group)
     R0E53036ACFK40 (Converter board for the R8C/36X groups)



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal