Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on Sep. 1, 2008: 080901/tn1

A Note on Using High-performance Embedded Workshop


Please take note of the following problem in using High-performance Embedded Workshop (High-performance Embedded Workshop is bundled with the software products such as compilers and emulator debuggers that it manages):
  • With using Replace and Find functions


1. Product and Versions Concerned
   All the versions of High-performance Embedded Workshop

2. Descriptions
2.1 Replace Functions
    Open the Edit menu and select the Replace command. Then in the dialog 
    box that appears, type a 2-byte character code into the Find what or 
    Replace with text box, check the Regular expression check box, and 
    click the Replace button. And you will see the code will be replaced 
    with an incorrect character string.
    If you click the Replace All button instead of the Replace button, 
    High-performance Embedded Workshop may be terminated abnormally.

2.2 Finding Text Functions 
    Open the Edit menu and select the Find command. Then in the dialog box 
    that appears, type a 2-byte character code into the Find what text 
    box, check the Regular expression check box, and click the Find Next 
    button. And you may obtain an incorrect search result.

    The character string searched for is highlighted in the Source window.
    Besides the above problem, however, the highlighted character string 
    and the character strings before and after it may be replaced with 
    incorrect ones.

    If you save the source file, the character string searched for and 
    those before and after it will remain as replaced with incorrect ones.

3. Workaround
   If you use a 2-byte character code in Find what or Replace with text 
   box, uncheck the Regulare Expression check box (disable the Regulare 
   Expression function).

4. Schedule of Fixing the Problem
   We plan to fix this problem in our future release.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal