Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on Sep. 1, 2008: 080901/tn6

E10A-USB Emulator Software Revised to V.2.13 Release 00


We have revised the emulator software for the E10A-USB emulators HS0005KCU01H and HS0005KCU02H from V.2.12 Release 00 to V.2.13 Release 00. The emulator software and these emulators are used for the SuperH RISC engine, H8S, and H8SX families of MCUs.

1. Product and Versions to Be Updated
   The emulator software for the E10A-USB emulators HS0005KCU01H and 
   HS0005KCU02H V1.0.00 through V.2.12 Release 00

2. Descriptions of Revision
2.1 Supported Devices Increased
    The following devices have been added to the support line:
Device Group Devices
H8SX H8SX/1638LF, H8SX/1634LF, H8SX/1632LF,
  H8SX/1648LF, H8SX/1644LF, H8SX/1642LF,
  H8SX/1648GF, H8SX/1644GF, H8SX/1642GF,
  H8SX/1648HF, H8SX/1644HF, H8SX/1642HF,
  H8SX/1658MF, H8SX/1654MF, H8SX/1653MF,
  H8SX/1668MF, H8SX/1664MF, and H8SX/1663MF
2.2 Start/Stop Function Improved
    The Start/Stop function, introduced in V.2.11 Release00 and 
    V.2.12 Release 00, has been improved so that the function can be 
    used in emulating the systems with the H8S and H8SX device groups.
    For details of this function, see RENESAS TOOL NEWS Document No. 
    080301/tn3 at:
        http://tool-support.renesas.com/eng/toolnews/080301/tn3.htm

2.3 Problem Fixed
    The following problem has been fixed:
    - When the systems with the SH-4A or New_SH-Mobile device group is 
      debugged with little endian format selected, the monitor window 
      (the one for monitoring memory contents during execution of 
      the user program) cannot be updated.

3. How to Update Your Product
   Free-of-charge online update is available. Use AutoUpdate Utility 
   on and after September 5; otherwise use the following procedure:
   
   (1) Download the update program of the product (a ZIP file) from:
          http://www.renesas.com/e10a_usb_download
       This site will be opened from September 5 on.
       The above URL is that of our global site (in English).

       Two types of update program are available. The one consists of the 
       update programs each of which is downloaded individually for the 
       corresponding device group supported by the E10A-USB emulators. 
       The other, the full-package edition, consists of those that can be 
       downloaded at a time for all the device groups. Use either of them.
	   
   (2) Decompress the downloaded ZIP file to obtain the install programs; 
       then execute it.
       If you have downloaded the full-package edition of the update 
       programs, you will obtain the HewInstMan.exe file, and if the other, 
       setup1.exe, after decompression.

4. Notice
   If either of the installer programs is executed in the development 
   system where High-performance Embedded Workshop V.4.04.00 or earlier 
   resides, it will be upgraded to V.4.04.01.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal