Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on Sep. 16, 2008: 080916/tn1

A Note on Using High-performance Embedded Workshop V.4.04.01


Please take note of the following problem in using High-performance Embedded Workshop V.4.04.01:
  • On the function for tree view of source files displayed when debug-only project is used

High-performance Embedded Workshop is bundled with the compilers and other software products that it manages. To check to see the version number of your High-performance Embedded Workshop, open the Help menu and select the About High-performance Embedded Workshop command.

1. Description
   When load module files are loaded onto the emulator debugger or 
   simulator debugger, the Locate Files dialog box appears. In this dialog 
   box even if the Look in subdirectries check box is checked on, no 
   searches are made through the subdirectories.

   The Locate Files dialog box opens only if any debug-only project 
   (the name of project type: Debugger only - xxxxxx) is used, and 
   the actual path to any load module file cannot 
   be found using the path information on the source files contained in 
   the debug information of the load module files.

   For details of the Locate Files functions, see the 
   "Showing a source tree on download" page in the help library of 
   High-performance Embedded Workshop.

2. Workaround
   Select the subdirectory to search, and then search for files.

3. Schedule of Fixing the Problem
   We plan to fix this problem in the next release of the product.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal