1. Product and Versions Concerned
All the versions of High-performance Embedded Workshop up to V.4.04.01
2. Description
If you search more than one file for a character string, the file name,
line number, and others of the character string searched for may be
displayed in white in the Output window, resulting in those being not
legible.
When you continue searching for character strings after this problem
has occurred, close High-performance Embedded Workshop once and then
restart it.
To search more than one file for a character string
1. On the Edit menu, select Find In Files.
2. Enter or select the necessary item(s) in the Find In Files dialog
box.
For further information, see the user's manual of High-performance
Embedded Workshop.
3. Schedule of Fixing the Problem
We plan to fix this problem in the next release of the product.