1. Product and Versions Concerned
All the versions of High-performance Embedded Workshop up to V.4.04.01
2. Description
When any files are selected out of a list in the Add files to project
'project name' dialog box to add them to a project, it cannot be added
with an error message being displayed if the file name contains more than
50 characters.
To open the Add files to project 'project name' dialog box
- On the Project menu, select Add Files.
For further information, see the user's manual of High-performance
Embedded Workshop.
3. Workaround
When the name of a file contains more than 50 characters, add the file
to a project as follows:
- Drag and drop the file to be added from Windows(R) Explorer onto
the icon of the project in the Workspace window of High-performance
Embedded Workshop.
4. Schedule of Fixing the Problem
We plan to fix this problem in the next release of the product.