1. Product and Versions Concerned
High-performance Embedded Workshop V.4.01.01 through V.4.04.01
To check to see the version number of your High-performance Embedded
Workshop, open the Help menu and select the About High-performance
Embedded Workshop command.
2. Description
If two or more modules have been registered in the Download modules
list, which appears in the Debug Settings dialog box (NOTE 1), those
modules are loaded according to the registered order in this list when
you load them at a time (NOTE 2).
However, this order is not kept once the active workspace is closed,
and it is changed to alphabetical order when the workspace is re-opened.
So if you load two or more modules at a time, they will be loaded in
alphabetical order this time.
NOTES:
1. To open the Debug Settings dialog box, open the Debug menu and
click Debug Settings.
2. To load two or more modules, open the Debug menu and click
Download Modules and then click All Download Modules.
3. Workaround
To modify the order of loaded modules as you like, do so in the
Download modules list after opening a workspace. While the workspace
is open, the modified order in the Download modules list will
be kept.
4. Schedule of Fixing the Problem
We plan to fix this problem in the next release of the product.