1. Product and Versions Concerned
All the versions of High-performance Embedded Workshop up to V.4.04.01
2. Description
If the version number of the toolchain used for the active workspace
is changed (NOTE 1), the settings of options in all the input files
that are displayed in the tree view of the build options dialog box for
custom build phases (NOTE 2) may be changed to the settings
made to Default Options that are also displayed in the above tree view.
NOTES:
1. To change the version number of a toolchain, make the change
when starting High-performance Embedded Workshop, or open the
Tools menu and select the Change Toolchain Version command.
This command can be selected if a toolchain to which the toolchain
used to create the project is upgradable has already been
registered with High-performance Embedded Workshop.
2. To open the build options dialog box for custom build phases,
open the Build menu and click the name of the custom build phase.
3. Workaround
If you have changed the version number of the toolchain that is used
for a workspace containing custom build phase where the necessary
build options are set to each input file, re-set the build options
for the custom build phase.
4. Schedule of Fixing the Problem
We plan to fix this problem in the next release of the product.