1. Products to Be Updated
(1) For the SH-4 and SH-4A CPU-cored MCUs
HI7750/4 V.2.01 Release 00 through V.2.02 Release 04
(2) For the SH4AL-DSP, SH-3, and SH3-DSP CPU-cored MCUs
HI7700/4 V.2.01 Release 00 through V.2.03 Release 02
2. Description of Revision
The problems have been fixed in both products, of which we informed you
in RNESAS TOOL NEWS Document No. 081101/tn2, "Notes on Using the Real-
Time OSes--HI7750/4 and HI7700/4--for the SuperH MCU Family."
For details of the problem, see the above item of news on the Web
page at:
http://tool-support.renesas.com/eng/toolnews/081101/tn2.htm
This Web page will be opened from November 6 on.
3. Updating Your Products and Purchasing the Revised Ones
3.1 Updating
When you are using either of the products to be updated, online update
is available free of charge.
Download the installer of the revised product you want from the
following Web sites at:
(1) For HI7750/4 V.2.02 Release 05
http://www.renesas.com/hi7750_4_download
(2) For HI7700/4 V.2.03 Release 03
http://www.renesas.com/hi7700_4_download
Then execute it. These Web sites will be opened from November 6 on.
The above URLs are that of our global site (in English).
NOTICE:
Updating from V.1 to V.2 is unavailable. If you are using a V.1
product, please place the order for the latest version you want.
3.2 First Ordering
When you place an order for the product you want, supply the following
items of information to your local Renesas Technology sales office or
distributor:
(1) HI7750/4
| Product type: |
HI7750/4 |
| Type Name: |
R0R40775TRW02w |
| Version No.: |
V.2.02 |
| Release No.: |
Release 05 |
| Host OS: |
Windows XP or Windows 2000 |
(2) HI7700/4
| Product type: |
HI7700/4 |
| Type Name: |
R0R40770TRW02w |
| Version No.: |
V.2.03 |
| Release No.: |
Release 03 |
| Host OS: |
Windows XP or Windows 2000 |
For the prices of the products, ask the above sales office or
distributor.
NOTICE:
Letter w denotes the types of license. It shall be replaced with
any one of the following numerals or letters:
1: |
Evaluation license; a real-time OS can be installed only
to one host computer. |
5: |
Evaluation license; a real-time OS can be installed
up to 5 host computers. |
A: |
Evaluation license; a real-time OS can be installed
up to 10 host computers. |
K: |
Mass-production license; a real-time OS can be embedded up to
a total of 1,000 productions of product model(s) with the source
code not disclosed. |
U: |
Mass-production license; a real-time OS can be embedded up to
unlimited productions of product model(s) with the source code
not disclosed. |
Z: |
Mass-production license; a real-time OS can be embedded up to
unlimited productions of product model(s) with the source code
disclosed. |
Example:
For mass-production license up to a total of 1,000 productions
designed with any of the SH-4 CPU-cored MCUs with the source code
not disclosed, the type name is R0R40775TRW02K.