1. Descriptions of Revision
1.1 Functions Introduced
(1) Mutex and message buffer
Service calls concerning mutex and message buffer can be issued.
(2) Checking parameters
As return values of service calls, E_ID, E_PAR, and E_CTX have been
supported. So the kernel's error detection capability has been
enhanced.
(3) Calling the system-down routine
The system-down routine can be called if inevitable errors arise
in the user program.
(4) Debugging OS
When M3T-MR100/4 is used with E30A Emulator Debugger V.1.01
Release 00, which is going to be published on June 1, 2009,
the following OS debugging functions can be used:
- MR tracing
- MR analyzing
- Issuing service calls
1.2 Problems Fixed
The following known problems have been fixed. For details of these,
see the respective RENESAS TOOL NEWS items.
(1) With issuing the pol_sem and ipol_sem service calls
RENESAS TOOL NEWS Document No. 080901/tn4
http://tool-support.renesas.com/eng/toolnews/080901/tn4.htm
(2) With using the cyclic and alarm handlers
RENESAS TOOL NEWS Document No. 080901/tn4
http://tool-support.renesas.com/eng/toolnews/080901/tn4.htm
(3) Correction to stack usage calculation methods
RENESAS TOOL NEWS Document No. 081116/tn1
http://tool-support.renesas.com/eng/toolnews/081116/tn1.htm
(4) With using the timeout function
RENESAS TOOL NEWS Document No. 090516/tn2
http://tool-support.renesas.com/eng/toolnews/090516/tn2.htm
(to be opened on and after June 5, 2009)
(5) With placing a fixed-length memory pool in a memory area
RENESAS TOOL NEWS Document No. 090516/tn2
http://tool-support.renesas.com/eng/toolnews/090516/tn2.htm
(to be opened on and after June 5, 2009)
2. How to Update Your product and
Purchase the Revised One
2.1 Updating
Online update is available free of charge.
To update yours, download the installer of the V.1.01 Release 00
product from the Web site at:
http://www.renesas.com/mr100_4_download
This site will be opened from June 5, 2009, on.
2.2 First Ordering
When you place an order for the product, supply the following items
of information to your local Renesas Technology sales office or
distributor:
| Product Type: |
M3T-MR100/4 (evaluation license), or
M3T-MR100/4 (mass-production license) |
| Type Name: |
R0R56400TRW01wE |
NOTE:
Letter w denotes a type of license. It shall be replaced with
any one of the following numerals or letters:
1: |
Evaluation license: The real-time OS can be installed only
to one host computer. |
5: |
Evaluation license: The real-time OS can be installed
up to 5 host computers. |
A: |
Evaluation license: The real-time OS can be installed
up to 10 host computers. |
K: |
Mass-production license: The real-time OS can be embedded up to
a total of 1,000 productions of product model(s) with the source
code not disclosed. |
U: |
Mass-production license: The real-time OS can be embedded up to
unlimited productions of product model(s) with the source code
not disclosed. |
Z: |
Mass-production license: The real-time OS can be embedded up to
unlimited productions of product model(s) with the source code
disclosed. |
Example:
For mass-production license up to a total of 1,000 productions for
any MCU of the R32C/100 series with the source code not disclosed,
the type name is R0R56400TRW01KE.