Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on June 4, 2009: 090604/tn1

An MCU Unit--R0E417250MCU00--
for the E100 Emulator Released


We have released an MCU unit--R0E417250MCU00--for the E100 emulator, which is used to evaluate and debug systems designed with MCUs of the H8SX/1720 group, H8SX/1700 series.

1. Features of the Product
   The R0E417250MCU00 MCU unit is used in combination with the E100 
   emulator to evaluate and debug systems designed with members of 
   the H8SX/1720 group, H8SX/1700 series of Renesas 32-bit MCUs.
   For details of the product, see:
     http://www.renesas.com/e100/r0e417250mcu00
   And for information on the E100 emulator, see:
     http://www.renesas.com/e100

   The above URLs are that of our global site (in English). 

   To debug your systems, you need to use an optional converter board 
   for connecting the target system with the flexible cable attached to 
   the unit. 
      Type name of the converter board:
            R0E0100TNPFK00
      This converter board connects the flexible cable with the 
      PLQP0100KB-A package (previous FP-100U and FP-100UV), which is 
      used for the H8SX/1720 MCU group.

   For details of the R0E0100TNPFK00 converter board, see its manual on 
   the Web page at:
     http://documentation.renesas.com/eng/products/tool/rej10j1736_r0e0100tnpfk00_u.pdf

2. The Contents of the Product Package
   The product package contains the following:
   (1) An MCU unit--R0E417250MCU00
   (2) A flexible cable (already connected with the MCU unit)
   (3) An 8-MHz oscillator module (already mounted on the MCU unit)
   (4) A CD-ROM containing H8SX E100 Emulator Software V.1.00 Release 01
       For details of the functionality of the software, see from here.
        
3. How to Purchase the Product
   When you place an order for the product, supply the following items 
   of information to your local Renesas Technology sales office or 
   distributor:
      Product type:  R0E417250MCU00 (MCU unit)
      Type name:     As above

      Product type:  R0E0100TNPFK00 (Converter board)
      Type name:     As above

   For the price of the product, also contact the above sales office or 
   distributor. 




© 2003-2010 Renesas Technology Corp., All rights reserved. Web Site Usage Conditions| Privacy| Sitemap