Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on June 4, 2009: 090604/tn2

H8SX E100 Emulator Software Published


We have published H8SX E100 Emulator Software V.1.00 Release 01.

1. Outline
   H8SX E100 Emulator Software is the software for controlling the E100 
   emulator, which is used in combination with the E100 emulator and 
   R0E417250MCU00 MCU unit (see NOTE) to evaluate and debug systems 
   designed with MCUs of the H8SX/1700 series.
   This emulator software is included with the product package of the 
   R0E417250MCU00 MCU unit; not available alone.

    NOTE
      This MCU unit, released on June 4, 2009, is used for the H8SX/1720 
      MCU group. For details of the unit, see Renesas Tool News Document 
      No. 090604/tn1, published on June 4, 2009, at
        http://tool-support.renesas.com/eng/toolnews/090604/tn1.htm
      This Web page is opened from June 5 on.

2. Features
   Main features of the product are as follows:
   (1) User-friendly GUI (graphical user interface)
   (2) Quick, easy operations by dragging and dropping
   (3) Fundamental debugging capabilities including source-level debugging 
       in C and assembly language.
   (4) Real-time RAM monitoring
   (5) High-performance debugging capabilities such as real-time tracing, 
       real-time profiling, coverage measurement, and time measurement
   (6) USB (USB 2.0 High-speed) supported
   (7) Online help in HTML

   For details of those features, see from here.

3. The Contents of the Product Package
   The package of H8SX E100 Emulator Software V.1.00 Release 01 contains 
   the following:
   (1) H8SX E100 Emulator Debugger V.1.00.01
   (2) High-performance Embedded Workshop V.4.05.01
   (3) AutoUpdate Utility V.1.05.00

4. Host System Requirements
     Computer:  IBM PC/AT or compatible
     OS:  Windows Vista(R), Windows(R) XP, or Windows(R) 2000
                Note, however, that the product does not run on the 64-bit 
                version of Windows Vista(R).

5. How to Get the Product
   This emulator software is included with the R0E417250MCU00 MCU unit.
   Also it can be downloaded from:
      http://www.renesas.com/e100_download
   This Web site is opened from June 5 on.

   The above URL is that of our global site (in English).

6. Notice
   If the emulator software is installed in the system where 
   High-performance Embedded Workshop V.4.04.01 or earlier resides, 
   this IDE will be updated to V.4.05.01. 


© 2003-2010 Renesas Technology Corp., All rights reserved. Web Site Usage Conditions| Privacy| Sitemap