|
|
 |
Download Site of the Beta Versions of USB drivers (for Renesas Emulators) Compatible
with the 64-Bit Edition of Microsoft Windows(R) 7
|
This site provides the USB drivers compatible with the
64-bit edition of Microsoft Windows(R) 7. Download the USB driver for the emulator and debugger which you use.
For information on how to install the USB Drivers, Read through the ReadMe file (in PDF) included in the download data.
Installer of the USB drivers (for Renesas Emulators) and
the ReadMe files
| Concerned Products |
Installer of
the USB driver |
Content |
| Emulator |
Emulator Debugger |
| E1 and E20 |
E1/E20 Emulator Software V.1.00 Release 00 and later |
Download
(ZIP 643KB) |
USB driver and ReadMe file |
| E100 |
H8S/Tiny E100 Emulator Software V.1.00 Release 00 and later |
Download
(ZIP 643KB) |
USB driver and ReadMe file |
M16C R8C E100 Emulator Software V.1.02 Release 00 and later |
Download
(ZIP 643KB) |
USB driver and ReadMe file |
| E8a |
E8a Emulator Software V.1.03 Release 00 and later |
Download
(ZIP 637KB) |
USB driver and ReadMe file |
| E30A |
R32C/100 E30A Emulator Debugger
V.1.01 Release 00 and later |
Download
(ZIP 643KB) |
USB driver and ReadMe file |
HS0005KCU01H and HS0005KCU02H (E10A-USB) |
E10A-USB Emulator Software
V.3.01 Release 00 and later (Note) |
Download
both of
(1) and (2),
and install them.
(1)Download
(ZIP 643KB)
(2)Download
(ZIP 637KB) |
USB driver and ReadMe file |
Note:
The E10A-USB Emulator Software is concerned only when any
MCUs in the following device groups are used as the target.
- The SH-2 device group
Except for the SH7615, SH7616, SH7047F, SH7144F, SH7145F,
SH7618, SH7619, SH7606 and SH7618A groups.
- The SH-2A device group
- The SH-4A device group
- The New_SH-Mobile device group
- The H8SX device group
- The H8S device group
Except for the H8S/2437, H8S/2114, H8S/2172, H8S/2158,
H8S/2189R, H8S/2116 and H8S/2125 groups.
|
 |