Skip to main content

Tool News

MCU unit for E100
Product Page: R0E530640MCU00 | R0E521300MCU00 | R0E530650MCU00 | R0E535M00MCU00 |
                               R0E420000MCU00 | R0E424270MCU00 | R0E556100MCU00 | R0E521500MCU00 |
See FAQs
See related news: High-performance Embedded Workshop
MCU File Download

Issue Date Title Description Device
Concerned
Apr. 1, 2012 Information about Free-of-Charge Upgrade of MCU Unit for E100 Emulator R0E521300MCU00 (Specific to R8C/3x Series, R8C Family) - R8C 
Jan. 16, 2012 M16C R8C E100 Emulator Software Revised to V.1.03 Release 02 V.1.03 Release 00 --> V.1.03 Release 02 -- 
Jan. 16, 2012 An MCU Unit for the E100 Emulator, R0E521500MCU00, Launched R0E521500MCU00: an MCU unit mounted to the E100 emulator, is used to debug systems designed with MCUs of the R8C/5x series. R8C/5x series
Jun. 16, 2011 M16C R8C E100 Emulator Software Revised to V.1.03 Release 01 V.1.03 Release 00 --> V.1.03 Release 01 M16C, R8C,
family
Apr. 27, 2011 A Note on Using M16C R8C E100 Emulator Software V.1.03 Release 00 (1) With using the MCU unit for the R8C/3x MCU series--R0E521300MCU00 R8C/3x
series
Mar. 29, 2011 M16C R8C E100 Emulator Software Revised to V.1.03 Release 00 V.1.02 Release 01 --> V.1.03 Release 00 M16C, R8C,
family
Dec. 16, 2010 A Note on Using the R0E420000MCU00 MCU Unit for the E100 Emulator (1) With displaying memory contents in real time in the RAM Monitor Window H8S/Tiny
series
Nov. 1, 2010 An MCU Unit for the E100 Emulator, R0E521300MCU00, Supports More MCUs In the R0E521300MCU00 MCU unit, the following groups of MCUs have been added to the support line.
R8C/33G, /33H, /32M, /33M, /34M, /34W, /34X,
/34Y, /34Z, /35M, /36W, /36X, /36Y, /36Z, /38W,
/38X, /38Y, and /38Z
R8C/3x
series
Sep. 16, 2010 RX E100 Emulator Software Published V.1.00 Release 00 RX600
series
Sep. 16, 2010 The MCU Unit R0E556100MCU00 for the E100 Emulator Marketed R0E556100MCU00: an MCU unit used for debugging systems designed with MCUs of the RX610 group, RX600 series, RX family. RX600
series
Aug. 16, 2010 H8SX E100 Emulator Software Revised to V.1.01 Release 00 V.1.00 Release 01 --> V.1.01 Release 00 H8SX family
Aug. 1, 2010 An MCU Unit--R0E424270MCU00--Used with the E100 Emulator Released R0E424270MCU00: an MCU unit used for debugging systems designed with MCUs of the H8S/2427, H8S/2427R, and H8S/2425 groups, H8S/2400 series. H8S/2400 series
Aug. 1, 2010 H8S/Tiny E100 Emulator Software Revised and Renamed V.1.00 Release 00 --> V.2.00 Release 00 H8S/Tiny,
H8S/2400
series
Jun. 16, 2010 A Note on Using H8S/Tiny E100 Emulator Software V.1.00 Release 00 With the memory access during execution of the user program. H8S/Tiny
series
Mar. 16, 2010 MCU Unit R0E521300MCU00 (Used for E100 Emulator) Supports More MCUs In the R0E521300MCU00 MCU unit, the R8C/34C group of MCUs have been added
to the support line.
R8C/3x series
Feb. 16, 2010 H8S/Tiny E100 Emulator Software Published H8S/Tiny E100 Emulator Software V.1.00 Release 00 H8S/Tiny
series
Feb. 16, 2010 An MCU Unit--R0E420000MCU00-- for the E100 Emulator Released R0E420000MCU00: an MCU unit used for debugging systems designed with MCUs of the H8S/Tiny series H8S/Tiny
series
Nov 16, 2009 MCUs Added to the Support Line of the R0E521300MCU00 MCU Unit (An MCU Unit Used with the E100 Emulator) In the R0E521300MCU00 MCU unit, which is used with the E100 emulator, the MCUs of the R8C/38C and R8C/36C groups have been added to the support line. R8C/3x series
Oct. 16, 2009 A Note on Using the MCU Unit R0E521300MCU00 in Combination with the E100 Emulator (1) With using several functions of the RD timer except Input Capture R8C/3x series
Oct. 1, 2009 MCUs Added to the Support Line of the R0E521300MCU00 MCU Unit (An MCU Unit Used with the E100 Emulator) In the R0E521300MCU00 MCU unit, which is used with the E100 emulator, the MCUs of the R8C/35C, /33C, /32C, /35D, /33D, and /32D groups have been added to the support line. R8C/3x series
Sep. 16, 2009 An MCU Unit--R0E535M00MCU00-- for the E100 Emulator Released R0E535M00MCU00: an MCU unit used for debugging systems designed with MCUs of the M16C/5M, M16C/5L, M16C/56, M16C/5LD, and M16C/56D groups, M16C/50 series M16C/50 series
Sep. 16, 2009 M16C R8C E100 Emulator Software Revised to V.1.02 Release 01 V.1.02 Release 00 --> V.1.02 Release 01 M16C, R8C,
family
Sep. 16, 2009 A Note on Using M16C R8C E100 Emulator Software and H8SX E100 Emulator Software (1) With using M16C R8C E100 Emulator Software or H8SX E100 Emulator Software in combination with High-performance Embedded Workshop V.4.06.00 or later on Windows Vista(R) M16C, R8C,
H8SX family
Aug. 16, 2009 A Note on Using M16C R8C E100 Emulator Software and a Correction to the User's Manual of the R0E530650MCU00 MCU Unit (1) Problem: With using the memory space expansion function (4Mbyte mode) of M16C R8C E100 Emulator Software in combination with the R0E530650MCU00 MCU unit
(2) Correction: To the last foot note on page 227 in the user's manual of the R0E530650MCU00 MCU unit
M16C/65, M16C/64A group
Jul. 16, 2009 M16C R8C E100 Emulator Software Revised to V.1.02 Release 00 V.1.01 Release 00 --> V.1.02 Release 00 M16C/50
series,
M16C/65 group
Jun. 16, 2009 Free-of-Charge Replacement of Malfunctioning Charged-WS, Commercial Products of the R0E530650MCU00 MCU Unit and Upgraded R0E530640MCU00 MCU Unit with Properly Functioning Ones In the charged-WS, commercial products of the R0E530650MCU00 MCU unit and the upgraded products of the R0E530640MCU00, we are replacing malfunctioning products with properly functioning ones free of charge. M16C/65, M16C/64A group
Jun. 4, 2009 H8SX E100 Emulator Software Published H8SX E100 Emulator Software V.1.00 Release 01 H8SX/1700
series
Jun. 4, 2009 An MCU Unit--R0E417250MCU00-- for the E100 Emulator Released R0E417250MCU00: an MCU unit for the E100 emulator, which is used to evaluate and debug systems designed with MCUs of the H8SX/1720 group, H8SX/1700 series. H8SX/1700
series
Apr. 1, 2009 Free of Charge Replacement of Malfunctioning Charged-WS2 and Commercial Products of the R0E521300MCU00 MCU Unit with Properly Functioning Ones In the charged-WS2 and commercial products of the R0E521300MCU00 MCU unit, replacing the malfunctioning products with the properly functioning ones free of charge. R8C/3x series
Apr. 1, 2009 An MCU Unit for the E100 Emulator R0E530640MCU00 (for the M16C/64 MCU Group) Upgradable with Extra Charge Upgrading an MCU unit for the E100 emulator R0E530640MCU00 (for the M16C/64 MCU group) to R0E530650MCU00 (for the M16C/65 and /64A MCU groups) with extra charge. M16C/64 group
Feb. 1, 2009 An MCU Unit--R0E521300MCU00--for the E100 Emulator Released (the MCU Unit Specific to the R8C/3x MCU Series) The R0E521300MCU00: an MCU unit used in combination with the E100 emulator for debugging systems designed with MCUs of the R8C/3x series R8C/3x series
Feb. 1, 2009 An MCU Unit--R0E530650MCU00-- for the E100 Emulator Released (the MCU Unit Specific to the M16C/65 and M16C/64A MCU Groups) The R0E530650MCU00: an MCU unit used in combination with the E100 emulator for debugging systems designed with MCUs of the M16C/65 and M16C/64A groups M16C/65,
M16C/64A
group
Feb. 1, 2009 M16C R8C E100 (Previous M16C E100) Emulator Software Revised to V.1.01 Release 00 V.1.00 Release 00 --> V.1.01 Release 00 M16C/60,
R8C/3x
series
Aug. 1, 2008 A Note on Using the R0E530640MCU00 --an MCU Unit for the E100 Emulator (1) Note of the problem described below in using the R0E530640MCU00, an MCU unit for the E100 emulator. M16C/64 group
May 20, 2008 A Note on Using the MCU Unit R0E530640MCU00 with the E100 Emulator (1) Note of the problem in using the MCU unit for the M16C/64 MCU group, R0E530640MCU0, with the E100 emulator. M16C/64 group
Apr. 16, 2008 M16C E100 Emulator Software V.1.00 Release 00 Published M16C E100 Emulator Software V.1.00 Release 00 has released. M16C/64 group
Apr. 16, 2008 An MCU Unit--R0E530640MCU00--for the E100 Emulator Released The R0E530640MCU00: an MCU unit used in combination with the E100 emulator for debugging systems designed with MCUs of the M16C/64 group M16C/64 group

In-circuit Emulator E100
Product Page
See FAQs
See related news: High-performance Embedded Workshop

Issue Date Title Description Device
Concerned
Mar. 1, 2012 Note on Using Renesas-Made Emulators --Problem with Using Emulators Connected to Windows 7-Installed PCs-- Problem with Using Emulators Connected to Windows 7-Installed PCs --
Feb. 1, 2008 Brand-New Full-Featured Emulator E100 Released Released a brand-new full-featured emulator--E100--for Renesas's 8- to 32-bit MCUs. --




End of content

Back To Top