Tool News
| On-Chip Debugging Emulator E8a | |
Tool News Search
System | |
| Issue Date | Title | Description | Device Concerned |
| Mar. 1, 2012 | Note on Using Renesas-Made Emulators --Problem with Using Emulators Connected to Windows 7-Installed PCs-- | Problem with Using Emulators Connected to Windows 7-Installed PCs | -- |
| Nov.16, 2011 | A Note on Using E8a Emulator Software | (1) With H8S/Tiny series MCU's data transfer controller (DTC) that is invoked during single-step execution or program break | H8S/Tiny series |
| Nov. 7, 2011 | E8a Emulator Software Revised to V.1.05 Release 01 | V.1.05 Release 00 to V.1.05 Release 01 | -- |
| Oct. 16, 2011 | A Note on Using E8a Emulator Software | (1) With debugging systems designed with MCUs of the H8S/Tiny series | H8S/Tiny series |
| Jul. 16, 2011 | A Note on Using E8a Emulator Software | (1) With the size of internal RAM accessible by the E8a emulator | R8C Family |
| Jun. 16, 2011 | E8a Emulator Software Revised to V.1.05 Release 00 | V.1.04 Release 00 to V.1.05 Release 00 | -- |
| Apr. 16, 2011 | Corrections to the Notes on Connecting MCUs of the R32C/100 Series --Additional Documents for the E8a Emulator User's Manual | (1) About corrections to the notes on connecting MCUs of the R32C/100 series--additional documents for the E8a emulator user's manual. | R32C/100 Series |
| Dec. 1, 2010 | A Note on Using the E8a and E8 Emulator Software Products | (1) With downloading programs extending over the data flash area and the program ROM or program ROM2 area; or manipulating data on memory in those areas | R8C Family, M16C Family |
| Nov. 26, 2010 | The E8a On-chip Debugging Emulator Supports More MCUs | MCU groups of the R8C/3x series, R8C family have been added to the support line. | R8C/3x series |
| Nov. 1, 2010 | A Note on Using E8a Emulator Software V.1.04 Release 00 | (1) With debugging systems designed with MCUs of the R8C/M11A or /M12A group | R8C Family |
| Jul. 6, 2010 | E8a Emulator Software Revised to V.1.04 Release 00 | V.1.03 Release 04 to V.1.04 Release 00 | -- |
| May 16, 2010 | A Note on Using E8a Emulator Software V.1.03 Release 04 | (1) With debugging systems designed with MCUs of the M16C/5M group encapsulated in a 100-pin package | M16C Family |
| Mar. 19, 2010 | A Note on Using E8a Emulator Software and E8 Emulator Software | (1) With performing step-over or step-out execution | M16C Family |
| Mar. 19, 2010 | E8a Emulator Software Revised to V.1.03 Release 04 | V.1.03 Release 03 to V.1.03 Release 04 | -- |
| Dec. 1, 2009 | A Note on Using E8a Emulator Software and E8 Emulator Software | (1) With executing commands for Memory Space Expansion Function 4MB Mode | M16C Family |
| Dec. 1, 2009 | E8a Emulator Software Revised to V.1.03 Release 03 | V.1.03 Release 02 to V.1.03 Release 03 | -- |
| Nov. 1, 2009 | A Note on Using E8a Emulator Software | (1) With running the self-check program E8aSCP.exe on Windows Vista(R) | -- |
| Oct. 1, 2009 | E8a Emulator Software Revised to V.1.03 Release 02 | V.1.03 Release 01 to V.1.03 Release 02 | -- |
| Sep. 16, 2009 | E8a Emulator Software Revised to V.1.03 Release 01 | V.1.03 Release 00 to V.1.03 Release 01 | -- |
| Aug. 1, 2009 | E8a Emulator Software Revised to V.1.03 Release 00 | V.1.02 Release 00 to V.1.03 Release 00 | -- |
| Feb. 1, 2009 | E8a Emulator Software Revised to V.1.02 Release 00 | V.1.01 Release 02 to V.1.02 Release 00 | -- |
| Jan. 9, 2009 | E8a Emulator Software Revised to V.1.01 Release 02 | V.1.01 Release 01 to V.1.01 Release 02 | -- |
| Sep. 1, 2008 | E8a Emulator Software Revised to V.1.01 Release 01 | V.1.01 Release 00 to V.1.01 Release 01 | -- |
| Jun. 16, 2008 | A Note on Using the Debuggers for the R8C/Tiny MCU Series | (1) With using the IO files for the R8C/2A, /2B, /2C, and /2D groups included in the debuggers for the R8C/Tiny MCU Series | R8C/Tiny |
| Apr. 1, 2008 | A Note on Using the E8a and E8 Emulator Software Products | (1) With debugging target systems designed with the M16C family of MCUs | M16C Family |
| Mar. 16, 2008 | A Note on Using the E8a and E8 Emulator Software Products | (1) With Debugging Systems Designed with Any Member of the M32C/80 MCU Series | M32C/80 MCU series |
| Feb. 16, 2008 | A Note on Using E8a Emulator Software V.1.01 Release 00 | (1) With debugging target systems designed with MCUs of the R8C/2G or R8C/2H group | R8C/2G, R8C/2H Group |
| Feb. 5, 2008 | E8a Emulator Software Revised to V.1.01 Release 00 | V.1.00 Release 00A to V.1.01 Release 00 | -- |
| Feb. 5, 2008 | A Note on Using E8a Emulator Software | (1) With Debugging Target Systems Designed with MCUs of the 38D5 Group | 38D5 Group |
| Feb. 5, 2008 | A Note on Using E8a Emulator Software | (1) With performing single-step execution in 740 E8a Emulator Debugger | 740 Families |
| Nov. 16, 2007 | A Note on Using the E8a and E8 Emulator Software Products | (1) Problem arising from a treatment of the MCU's pin connected with the BUSY pin on the emulator | 740, M16C Families |
| Oct. 1, 2007 | A Note on Using the Emulator Software Products for the E8a and E8 Emulators | (1) With Debugging Systems Designed with a Member of the R8C/22 Group of MCUs | R8C/22 group |
| Aug. 1, 2007 | E8a Emulator Software Revised to V.1.00 Release 00A | V.1.00 Release 00 to V.1.00 Release 00A | -- |
| Aug. 1, 2007 | A Note on Using E8a Emulator Software V.1.00 Release 00 |
(1) With Using the Evaluation Version of the C/C++ Compiler V.6.01 Release 03 for the H8SX, H8S, and H8 MCU Families Bundled with the Emulator Software | H8SX, H8S, and H8 MCU Families |
| Jul. 9, 2007 | The Brand-New On-Chip Debugging Emulator E8a will be Released | (Supported: Renesas's 8- to 32-bit MCUs) | -- |
|
|