Skip to main content

Tool News

Flash and PROM Programming:
Flash Development Toolkit | F-ZTAT On-board Programming Software |
    Adapter Board

Flash Development Toolkit
See FAQs
Technical Update
* Since Ver.4 is upward compatible with Ver.2 and Ver.3 and is supported by all Ver.2 and Ver.3 microcomputers, when Ver.4 begins to ship we will end the sale of Ver.2 and Ver.3.
* It cannot update from Ver.2 and Ver.3 to Ver.4. Please purchase the new version.


The news that had been issued on and after release date of
Flash Development Toolkit Ver.4 (R0C00000FDW04R)
Issue Date Title Description Fixed version
March 29, 2012 Flash Development Toolkit Revised to V.4.08 Release 01 V.4.08 Release 00 -> V.4.08 Release 01  
Mar. 1, 2012 Note on Using Renesas-Made Emulators --Problem with Using Emulators Connected to Windows 7-Installed PCs-- Problem with Using Emulators Connected to Windows 7-Installed PCs --
Oct. 31, 2011 Flash Development Toolkit Revised to V.4.08 Release 00 V.4.07 Release 01 -> V.4.08 Release 00  
Sep. 1, 2011 A Note on Using Flash Development Toolkit (1) With running the product on Microsoft Windows Vista or Windows 7 We have no plan to fix these problems.
Jul. 16, 2011 A Note on Using Flash Development Toolkit (1) With running the product on Windows Vista or Windows 7 We have no plan to fix these problems.
Jun. 30, 2011 Flash Development Toolkit Revised to V.4.07 Release 01 V.4.07 Release 00 -> V.4.07 Release 01  
May 16, 2011 A Note on Using Flash Development Toolkit (1) With using script command Exit V.4.07 Release 01
Mar. 16, 2011 Flash Development Toolkit Revised to V.4.07 Release 00 V.4.06 Release 01 -> V.4.07 Release 00  
Feb. 16, 2011 A Correction to User's Manuals of Flash Development Toolkit We inform you about a correction to the User's Manuals of Flash Development Toolkit V.3.06 Release 00 through V.4.06 Release 01. --
Feb. 1, 2011 Notification about Ending Support for Flash Development Toolkit Versions 2 and 3 We are ending support for Flash Development Toolkit versions 2 and 3. --
Nov. 29, 2010 A Note on Using Flash Development Toolkit (1) With programming data flash areas V.4.07 Release 00
Nov. 29, 2010 A Note on Using Flash Development Toolkit (1) With the ID Code dialog box being displayed V.4.06 Release 00
Nov. 29, 2010 A Note on Using Flash Development Toolkit (1) With successively programming flash memory by using the E8a in the E8aDirect mode V.4.07 Release 00
Nov. 29, 2010 A Note on Using Flash Development Toolkit (1) With using the Request Checksum and Readback Verify options V.4.07 Release 00
Nov. 16, 2010 Flash Development Toolkit Revised to V.4.06 Release 01 V.4.06 Release 00 -> V.4.06 Release 01  
Nov. 1, 2010 A Note on Using Flash Development Toolkit V.4.06 Release 00 (1) With using the E1 or E20 emulator as a flash programmer V4.06 Release 01
Aug. 5, 2010 Flash Development Toolkit Revised to V.4.06 Release 00 V.4.05 Release 01 -> V.4.06 Release 00  
May 25, 2010 A Note on Using Flash Development Toolkit (1) With programming to MCUs of the M16C/6B, /56, and /5L groups V4.06 Release 00
Apr. 16, 2010 A Note on Using Flash Development Toolkit (1) With performing the forced erase function in the M16C MCU family V4.06 Release 00
Apr. 16, 2010 Flash Development Toolkit Revised to V.4.05 Release 01 V.4.05 Release 00 -> V.4.05 Release 01  
Apr. 1, 2010 A Note on Using Flash Development Toolkit (1) With using the toolkit in the Basic Simple Interface Mode V.4.05 Release 01
Mar. 16, 2010 A Note on Using Flash Development Toolkit (1) With Erasing Flash Memory V.4.05 Release 00
Mar. 16, 2010 A Note on Using Flash Development Toolkit (1) With Selecting a Programming Destination V.4.05 Release 01
Feb. 22, 2010 Flash Development Toolkit Revised to V.4.05 Release 00 V.4.04 Release 00 -> V.4.05 Release 00  
Dec. 16, 2009 Flash Development Toolkit Revised to V.3.07 Release 05 V.3.07 Release 04 -> V.3.07 Release 05  
Oct. 29, 2009 Flash Development Toolkit Revised to V.4.04 Release 00 V.4.03 Release 02 -> V.4.04 Release 00  
Oct. 29, 2009 A Note on Using Flash Development Toolkit (1) Problem with block-erasing of flash ROMs in the 96-KB version of the R8C/Lx series, R8C family of MCUs
(2) With using MCUs in the USB Boot mode
V.4.04 Release 00
Oct. 1, 2009 Flash Programmer HS0008EASF5H Published - -
Oct. 1, 2009 A Note on using Flash Development Toolkit V.3 Note on Using Flash Development Toolkit V.3 V.3.07 Release 05
Aug. 7, 2009 Flash Development Toolkit Revised to V.4.03 Release 02 V.4.03 Release 01 -> V.4.03 Release 02  
Apr. 8, 2009 Flash Development Toolkit Revised to V.4.03 Release 01 V.4.03 Release 00 -> V.4.03 Release 01  
Mar. 5, 2009 A Note on Using Flash Development Toolkit V.4.03 Release 00 With executing "Readback Verify" and "Request Checksum" after the flash ROM of the device is programmed. V.4.03 Release 01
Jan. 30, 2009 Flash Development Toolkit Revised to V.4.03 Release 00 V.4.02 Release 01 -> V.4.03 Release 00  
Dec. 25, 2008 A Note on Using Flash Development Toolkit With executing Flash Development Toolkit in Basic mode V.4.03 Release 00
Oct. 16, 2008 Flash Development Toolkit Revised to V.4.02 Release 01 V.4.02 Release 00 -> V.4.02 Release 01  
Jul. 28, 2008 Flash Development Toolkit Revised to V.4.02 Release 00 V.4.01 Release 01 -> V.4.02 Release 00  
Jun. 16, 2008 A Note on Using Flash Development Toolkit Note in using Flash Development
Toolkit in combination with the E8a emulator
V.4.02 Release 00
May 16, 2008 A Note on Using Flash Development Toolkit With taking "E8aDirect" as arguments of the "connect" script command V.4.02 Release 00
Apr. 4, 2008 Flash Development Toolkit Revised to V.4.01 Release 01 V.4.01 Release 00 -> V.4.01 Release 01  
Jan. 16, 2008 Flash Development Toolkit Revised to V.4.01 Release 00 V.4.00 Release 02 -> V.4.01 Release 00  
Nov. 16, 2007 Flash Development Toolkit Revised to V.3.07 Release 04 V.3.07 Release 03 -> V.3.07 Release 04  
Oct. 12, 2007 Flash Development Toolkit Revised to V.4.00 Release 02 V.4.00 Release 01 -> V.4.00 Release 02  
Sep. 16, 2007 A Note on Using Flash Development Toolkit With programming the internal QzROM of QzROM-version MCUs in the 740 family V.4.00 Release 02
V.3.07 Release 04
Aug. 1, 2007 Flash Development Toolkit Revised to V.4.00 Release 01 V.4.00 Release 00 -> V.4.00 Release 01  
Aug. 1, 2007 Flash Development Toolkit Revised to V.3.07 Release 03 V.3.07 Release 02 -> V.3.07 Release 03  
Aug. 1, 2007 A Note on Using Flash Development Toolkit With Programming Memory on the Flash-Version MCUs of the 740 Family
Using the E8 On-Chip Debugging Emulator
V.4.00 Release 01
Jul. 16, 2007 A Note on Using Flash Development Toolkit V.4.00 Notes on Using Flash Development Toolkit V.4.00 V.4.01 Release 00
Jul. 1, 2007 Notes on Using Flash Development Toolkit Notes on Using Flash Development Toolkit V.3.05 through V.3.07 We have no plan to fix these problems.
Jun. 16, 2007 Flash Development Toolkit Revised to V.4.00 Release 00 V.3.07 Release 02 -> V.4.00 Release 00  


The news that had been issued on and after release date of
Flash Development Toolkit Ver.3 (HS6400FDIW3SR)
Issue Date Title Description
Feb. 23, 2007 The Uninstaller for the Flash Development Toolkit V.3.06 and V.3.07 Released The uninstaller for the Flash Development Toolkit V.3.06 and V.3.07 has been released.
Feb. 23, 2007 The Flash Development Toolkit Revised to V.3.07 Release 02 V.3.07 Release 01 -> V.3.07 Release 02
Dec. 21, 2006 The Flash Development Toolkit Revised to V.3.07 Release 01 V.3.07 Release 00 -> V.3.07 Release 01
Dec. 21, 2006 A Note on Uninstalling the Flash Development Toolkit V.3.06 Release 00 and V.3.07 Release 00 On uninstalling the Flash Development Toolkit V.3.06 Release 00 and V.3.07 Release 00
Nov. 1, 2006 The Flash Development Tool Kit Revised to V.3.07 Release 00 V.3.06 Release 00 -> V.3.07 Release 00
May. 16, 2006 The Flash Development Toolkit Revised to V.3.06 Release 00 V.3.05 Release 01 -> V.3.06 Release 00
Jan. 16, 2006 The Flash Development Toolkit Revised to V.3.05 Release 01 V.3.05 Release 00 -> V.3.05 Release 01
Dec. 1, 2005 A Note on Using the Flash Development Toolkit V.3.05 Release 00 On programming any of the H8/300L Super Low Power series of MCUs
Oct. 16, 2005 Flash Development Toolkit Revised to V.3.05 Release 00 V.3.04 Release 00 -> V.3.05 Release 00
May. 1, 2005 Flash Development ToolKit Revised to V.3.04 Release 00 Ver3.3 -> V.3.04 Release 00
-- Release Information of Flash Development ToolKit Ver.3.3 Ver3.2 -> Ver3.3
-- Release Information of Flash Development ToolKit Ver.3.2 Ver3.1 -> Ver3.2
-- Release Information of Flash Development ToolKit Ver.3.1 Ver3.0 -> Ver3.1
-- Release Information of Flash Development ToolKit Ver.3.0 Ver3.00

The news that had been issued on and after release date of
Flash Development Toolkit Ver.2 (HS6400FDIW2SR)
Issue Date Title Description
-- Release Information of Flash Development ToolKit Ver.2.2.005 Ver.2.2.004 -> Ver.2.2.005
-- Release Information of Flash Development ToolKit Ver.2.2.004 Ver.2.2.003 -> Ver.2.2.004
-- Release Information of Flash Development ToolKit Ver.2.2.003 Ver.2.2.001 -> Ver.2.2.003
-- Release Information of Flash Development ToolKit Ver.2.2.001 Ver.2.2 -> Ver.2.2.001
-- Release Information of Flash Development ToolKit Ver.2.2 Ver.2.1 -> Ver.2.2
-- Release Information of Flash Development ToolKit Ver.2.1 Ver.2.0.001 -> Ver.2.1
-- Release Information of Flash Development ToolKit Ver.2.0.001 Ver.2.0.001


F-ZTAT On-board Programming Software
See FAQs
Technical Update
* This product (HS6400FWIW ...) is a product of each version outright sale. In case you use a new version, please purchase newly.

Ver.5 (HS6400FWIW5SR)
Issue Date Title Description
-- Release Information of F-ZTAT On-board Programming Software Ver.5.0C Ver.5.0B -> Ver.5.0C
-- Release Information of F-ZTAT On-board Programming Software Ver.5.0B Ver.5.0A -> Ver.5.0B
-- Release Information of F-ZTAT On-board Programming Software Ver.5.0A Ver.5.0 -> Ver.5.0A
-- Release Information of F-ZTAT On-board Programming Software Ver.5.0 Ver.5.0

Ver.4 (HS6400FWIW4SR)
-- Release Information of F-ZTAT On-board Programming Software Ver.4.0 Ver.4.0

Ver.3 (HS6400FWIW3SR)
-- Release Information of F-ZTAT On-board Programming Software Ver.3 (1) Ver.3.0
(2) Ver.3.0 -> Ver.3.1


Adapter Board
See FAQs
Technical Update

Issue Date Title Description
Oct. 1, 2009 Flash Programmer HS0008EASF5H Published HS0008EASF5H
Jun. 1, 2009 A Note on Using the Flash Programmer HS0008EASF4H and Notification of Modifying Specifications HS0008EASF4H
Jun. 1, 2009 A Note on Using the Flash Programmer HS0008EAUF1H and Notification of Changing Programming Tools HS0008EAUF1H




End of content

Back To Top