|
|
 |
Flash Development Toolkit Ver3.0
Flash development toolkit Ver3.0 added the following function to Ver.2.0.
An additional function
- The [support device inquiry] command corresponding to 0.18-micrometer
product is added.
Also to the microcomputer released from now on, writing becomes
possible, without upgrading.
- The sum value display function at the time of writing.
The program to write in can be checked.
- No. of an error message.
Please inform us of error message No. in the case of the inquiry
to a display support center.
- Add the disconnect button to Simple interface.
It becomes easy to carry out continuation writing.
|
 |