Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
F-ZTAT On-board Programming Software

  Ver.3.1 release Information

host's (FLASH.EXE) changed part

  1. The file name specified to be a Write command dialog was changed so that it could be used also after a reboot.
  2. It changed so that all S type files created from the emulator (E7000 grade) could be analyzed.

  Ver.3.0 release information

host's (FLASH.EXE) changed part

  1. A change to the 32-bit version application was made, and it became possible to transmit user data at high speed. In addition, although operation on WindowsNT becomes possible from this version, it does not operate on Windows 3.1.
  2. Analysis processing of the Motorola S type file (user data) transmitted to a flash memory was changed, and the error output in case there is a debugging information (S4-S6) record was deterred.

Change and an addition of a device of a file

  • The new support (addition) of the following devices was carried out.
Series name Device name File name
H8/300
H8/3437SF
3437SF6
H8S
H8S/2194F
2194F6
SH
SH7017F
7017F6

© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal