Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
F-ZTAT On-board Programming Software Ver.5.0B

  Upgrade information

The F-ZTAT Microcomputer On-Board Writing Program has been updated from Ver. 5.0A to Ver. 5.0B.
The following components have been updated.

Update information from V5.0A to V5.0B

   1. Fixed programming error.

Target devices H8S/2142RF,H8S/2132RF and H8/3334F.
Flash programming error on Ver.5.0 and Ver.5.0A of Onboard Writing Program has been fixed on Ver.5.0B of it.

   2. Append supporting devices

H8/538F and H8S/2147NF are supported.

   3. For H8/538F users

In case of a user system, flash erasing time may spend over 5 seconds.
Then the Onboard Writing Program may displayed writing error(No.113) because of the default timeout setting(5 seconds). Please change timeout setting over 5 seconds, when this error message is displayed.

   4.How to update
  1. Please check that F-ZTAT microcomputer onboard writing program Ver.5.0A is already installed.
  2. An update program (UPV50B.exe) and ".inf", ".src", and ".sub" file are put on the directory (a default "C:program file\flash5\") to which it is installed in the F-ZTAT microcomputer onboard writing program (flash.exe).
  3. Please double-click and perform an update program (UPV50B.exe).

© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal