|
|
 |
F-ZTAT On-board Programming Software Ver.5.0C
The F-ZTAT microcomputer onboard writing tool was upgraded from Ver.5.0B to Ver.5.0C.
To update your products to the latest version 5.0C, the products need to be updated in order of old revisions. (5.0 > 5.0A > 5.0B > 5.0C)
How to upgrade
-
Please check that F-ZTAT microcomputer onboard write-in program Ver.5.0B is already installed.
-
An update program (UPV50C.exe) is put on the directory (a default "C:Program file\flash5\") to which it is installed in the F-ZTAT microcomputer onboard writing program (flash.exe).
-
Please double-click and perform an update program (UPV50C.exe).
-
If a normal end is carried out, it will be displayed as "Complete." When you do not carry out a normal end, please re-install master CD-ROM to Ver.5.0B, and carry out update procedure.
Known bug information
In SH7044F and SH7045F, although there was a phenomenon in which an error (NO.104 size error) was outputted at the time of writing control program transmission, it corrected.
|
 |