Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
H8/300H Tiny Compact Emulator Debugger
See Tool news for related products: High-performance Embedded Workshop | Compact Emulator
MCU File Download

Issue Date Title Description Status on the
Latest Version
Mar. 16, 2007 Three MCU Groups Newly Supported by the Compact Emulator R0E436640CPE00 for the H8/300H Tiny MCU Series The H8/36077, H8/36079, and H8/36094 MCU groups have become newly supported. --
Dec. 16, 2006 A Note on Using Debuggers for the SuperH RISC engine, M16C, H8SX, H8S, H8, and 740 MCU Families (1) With updating debuggers using the AutoUpdate Utility Not Fixed
Feb. 16, 2006 A Note on Using the H8/300H Tiny Compact Emulator Debugger V.1.00 Release 00 On downloading object files created by the compiler package for the H8SX, H8S, and H8 families Fixed
Feb. 16, 2006 The H8/300H Tiny Compact Emulator Debugger Revised to V.1.01 Release 00 V.1.00 Release 00 → V.1.01 Release 00 --
Jan. 16, 2006 A Note on Using the Debuggers for the M32R, M16C, H8 (H8/300H Tiny Series Only), and 740 MCU Families On referencing member variables of a structure, union, or class Fixed




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal