Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
High-performance Embedded Workshop Ver.3.0.02

The High-performance Embedded Workshop was updated to Ver.3.0.02 on December 15, 2003. Descriptions and how to update are shown below.


  Supported Products

This version supports the following products.
  • SuperH RISC engine C/C++Compiler packages
    • R0C40700XSW08R
    • P0700CAS7-MWR
  • M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, R8C/Tiny series
    • M3T-NC30WA Professional version
    • M3T-NC30WA Free version
  • H8S, H8/300 series C/C++Compiler packages
    • R0C40008XSW06R
    • PS008CAS5-MWR
  • E10A-USB emulators
    • HS0005KCU01H
    • HS0005KCU02H
  • E7 emulator
    • HS0007TCU01H

  Descriptions

  • Enhancement
    • Navigation function
      Category "C++ Classes" of the navigation function is unchecked as a default.
  • Problem Fixed
    • Problem fixed at termination
      We have fixed the problem that the IDE did not quit normally.

  Read This Before Downloading Update Program

The installer of the update program (hewv3002u.exe) released on November 20 had the following restrictions.
Therefore, we have fixed the problems and updated the program (hewv3002u2.exe) for the Ver.3.0.02 on December 15. Because we revised the installer only and the IDE is not modified, the version number is the same as the previous one.

And, if you have successfully installed the update program (hewv3002u.exe) released on November 20,
you do not need download the new update program (hewv3002u2.exe) released on December 15.

Restrictions of the Update Program (hewv3002u.exe)
for the Ver.3.0.02 Released on November 20.
  1. In the following cases, you cannot update the Ver.3.0.02.
    • Updated from Ver.1.0.00 to Ver.2.0.02
    • Updated from Ver.1.0.00 to Ver.2.0.02 (via Ver.2.0.01)
  2. With the following products, you cannot update the Ver.3.0.02.
    • Professional version and Free version
      of C compiler M3T-NC30WA for the M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, R8C/Tiny Series

© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal