On this page are described several notes on using the High-performance Embedded Workshop V.3.
Please read this page through if you are using any product associated with it.
[Introduction]
For details, click on the following image.

List of Products Associated with High-performance Embedded Workshop V.3
| A. |
Notes on Installing the High-performance Embedded Workshop V.3 |
|
The following problems that arise in the High-performance Embedded Workshop when two or more software products
(compiler packages, emulator software products, and updaters) reside in the same PC has been resolved in the High-performance Embedded Workshop V.3.01.04 and the High-performance Embedded Workshop V.3.01.05:
A-1. Problems Already Resolved in High-performance Embedded Workshop V.3.01.04
| No. |
Problem Resolved in High-performance Embedded Workshop V.3.01.04 |
Condition |
| (1) |
At invoking the High-performance Embedded Workshop, an application error appears. |
Refer to Condition. |
| (2) |
At invoking the High-performance Embedded Workshop, it cannot communicate with the emulator,
or the menu names for the emulator debugger cannot be displayed on the High-performance Embedded Workshop's menu bar. |
Refer to Condition. |
| (3) |
In the New Project Workspace dialog box, the Tool chain drop-down list box becomes inactive, so no tool chains are selectable. |
Refer to Condition. |
| (4) |
If any tool chain is selected in the Tool chain drop-down list,
project types for builds cannot be displayed in the Project Type list box of the New Project Workspace dialog box. |
Refer to Condition. |
| (5) |
A project type "Debugger Only" for the emulator will not appear
in the Project type list box of the New Project Workspace dialog box. |
Refer to Condition. |
If any of the above problems arises in your High-performance Embedded Workshop,
update it to the High-performance Embedded Workshop V.3.01.04 or later by using the updater (yours is overwritten).
The latest High-performance Embedded Workshop updater supports other problems in addition to "Problems Already Resolved in High-performance Embedded Workshop V.3.01.04".
Therefore, various problems can be solved only by installing the latest High-performance Embedded Workshop updater once.
A-2. Problems Already Resolved in High-performance Embedded Workshop V.3.01.05
| No. |
Problem Resolved in High-performance Embedded Workshop V.3.01.05 |
Condition |
| (1) |
No project types for builds cannot be displayed. |
Refer to Condition. |
If any of the above problems arises in your High-performance Embedded Workshop,
update it to the High-performance Embedded Workshop V.3.01.05 by using the updater (yours is overwritten).
This High-performance Embedded Workshop updater also supports "Problems Already Resolved in High-performance Embedded Workshop V.3.01.04".
Therefore, various problems can be solved only by installing this High-performance Embedded Workshop updater once.
| B. |
Notice regarding an upgrade to the latest compiler package |
|
This notice is intended for users of the SH:Ver.7.x or H8:Ver5.x compiler package other than the latest compiler package (SH:Ver7.1.03 / H8:Ver5.0.05). If you contemplate an upgrade to the latest version using an upgrade program distributed from our website, please note that HEW need to be upgraded to HEW3 by necessity. Please click here for details.
| C. |
Notice in case of using both of emulator, which High-performance Embedded Workshop V.2 is attached and compiler package |
|
If you are using both of emulators, which High-performance Embedded Workshop is attached to (E7 and some of E10A, E6000 and E6000H) and the latest version of compiler packages (SH:After Ver7.1.03 / H8:After Ver5.0.05), your emulator can be operated by HEW3 environment.
However, in case of installing emulator and compiler package in the same directory, in some cases, the emulator may not be connected, or, the project types to "Build" may be erased (So you can't build the project). In case that your emulator is not connected, you are required to follow particular procedures. Please click here for details.
| D. |
Notes on the Performance of the High-performance Embedded Workshop V.3 |
|
The High-performance Embedded Workshop V.3 may decrease in performance depending on its environmental conditions
since it provides a variety of functions. Here we introduce how to increase the High-performance Embedded Workshop's performance.
Please go to:
| E. |
Limitations on the High-performance Embedded Workshop Used in Combination with an Emulator |
|
If the High-performance Embedded Workshop V.3 is used in combination with an emulator,
some of the functions it supports may not be utilized depending on the type of emulator you use.
|