|
The list of the products associated with the High-performance Embedded Workshop 3 is shown below.
Here, the products associated with the High-performance Embedded Workshop 3 are those with which the High-performance Embedded Workshop 3 is included or those that can be updated to the High-performance Embedded Workshop 3 by using their updaters.
If several of them and the High-performance Embedded Workshop 3 are installed in the same PC, they can be managed through the High-performance Embedded Workshop 3 only.
NOTICE:
Be sure to install every of the products listed below and its managing High-performance Embedded Workshop into the same folder; otherwise, the product's operations cannot be guaranteed.
NOTE:
*1 For product types, please contact your nearest distributor.
*2 Involved are all the emulators listed in the High-performance Embedded Workshop Versions table in this download site.
|