|
|
 |
A Problem Already Resolved in the High-performance Embedded Workshop V.3.01.05
Updated on: August 20, 2004
| (1) |
No project types for builds cannot be displayed. |
|
Description
If any tool chain is selected in the Tool chain drop-down list, no project types for builds may not be displayed in the Project Type list box of the New Project Workspace dialog box (see the figure below).
Condition
After installing the SCH compiler package V.7.1.03 or later or the H8C compiler package V.5.0.05 or later, the E7 emulator software V.1.00 is installed without invoking the High-performance Embedded Workshop at all.
How to Fix the Problem
If the above problem arises in your High-performance Embedded Workshop,
update it to the High-performance Embedded Workshop V.3.01.05 by using the updater (yours is overwritten).
This High-performance Embedded Workshop updater also supports "Problems Already Resolved in High-performance Embedded Workshop V.3.01.04".
Therefore, various problems can be solved only by installing this High-performance Embedded Workshop updater once.
|
|
 |