|
|
 |
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Jun. 1, 2007 |
A Note on Using Debugger Products for the M16C and 740 Families of MCUs |
(1) With the Tooltip Watch function |
Not Fixed |
| Apr. 16, 2007 |
A Note on Using the Debuggers for the M16C Family;
the H8/300H Tiny Series, H8 Family; and the 740 Family of MCUs |
(1) With loading target programs on MCUs |
Not Fixed |
| Dec. 16, 2006 |
A Note on Using the Debuggers for the M32C MCU Series |
(1) With referencing values of IO register in the IO window |
Not Fixed |
| Dec. 16, 2006 |
A Note on Using Debuggers for the SuperH RISC engine, M16C, H8SX, H8S, H8, and 740 MCU Families |
(1) With updating debuggers using the AutoUpdate Utility |
Not Fixed |
| Sep. 16, 2006 |
The Debuggers for the M32C/90, M32C/80, M16C/80, and M16C/70 MCU Series Revised to Their V.1.02 Release 00
|
V.1.02 Release 00 |
-- |
| Sep. 16, 2006 |
A Note on Using the M32C Compact Emulator Debugger |
(1) On debugging programs that use the watch-dog timer function |
Not Fixed |
| Jan. 16, 2006 |
A Note on Using the Debuggers for the M32R, M16C, H8 (H8/300H Tiny Series Only), and 740 MCU Families |
(1) On referencing member variables of a structure, union, or class |
Fixed |
| Dec. 16, 2005 |
A Note on Using the M32C Compact Emulator Debugger V.1.00 Release 00 |
On changing the work area used by the compact emulator |
Fixed |
| Dec. 16, 2005 |
The M32C Compact Emulator Debugger Revised to V.1.00 Release 01 |
V.1.00 Release 00 → V.1.00 Release 01 |
-- |
| Oct. 1, 2005 |
The Emulator Debuggers for the M32C/80, and M16C/80 Series Published |
V.1.00 Release 00 |
-- |
|
 |