Tool News
| M32C PC7501 Emulator Debugger for M32C/80 Series | |
|
| |
| Issue Date | Title | Description | Status on the Latest Version |
| Apr. 1, 2008 | A Note on Using the PC7501 Emulator Debugger V.1.03 Release 00 for the M32C/90, M32C/80 and M16C/80 series of MCUs | (1) With displaying information on time in several windows | Not Fixed |
| July. 1, 2007 | The Debuggers for the M32C/90, M32C/80, and M16C/80 MCU Series
Revised to V.1.03 Release 00
|
V.1.02 Release 00 -> V.1.03 Release 00 | -- |
| Jun. 1, 2007 | A Note on Using Debugger Products for the M16C and 740 Families of MCUs | (1) With the Tooltip Watch function | Fixed |
| Apr. 16, 2007 | A Note on Using the Debuggers for the M16C Family; the H8/300H Tiny Series, H8 Family; and the 740 Family of MCUs |
(1) With loading target programs on MCUs | Fixed |
| Apr. 1, 2007 | The M30850T2-EPB Emulation Probe Supports More MCUs | (1) The M30850T2-EPB emulation probe has added all the members of the M32C/8A group, M32C/80 series, M16C family of MCUs to their support lines. | -- |
| Dec. 16, 2006 | A Note on Using the Debuggers for the M32C MCU Series | (1) With referencing values of IO register in the IO window | Fixed |
| Dec. 16, 2006 | A Note on Using Debuggers for the SuperH RISC engine, M16C, H8SX, H8S, H8, and 740 MCU Families | (1) With updating debuggers using the AutoUpdate Utility | Fixed |
| Sep. 16, 2006 | V.1.02 Release 00 | -- | |
| Jan. 16, 2006 | A Note on Using the Debuggers for the M32R, M16C, H8 (H8/300H Tiny Series Only), and 740 MCU Families | On referencing member variables of a structure, union, or class | Fixed |
| Oct. 1, 2005 | The Emulator Debuggers for the M32C/80, and M16C/80 Series Published | V.1.00 Release 00 | -- |
|
|