Skip to main content

Tool News

M32C Simulator Debugger
See Tool news for related products: High-performance Embedded Workshop | M3T-NC308WA

Issue Date Title Description Status on the
Latest Version
May 16, 2009

The Simulator Debugger for the M32C/80 and M16C/80 Series of MCUs Revised to V.1.04 Release 00

V.1.03 Release 00 -> V.1.04 Release 00 --
Jul. 1, 2007

The Debuggers for the M32C/90, M32C/80, and M16C/80 MCU Series Revised to V.1.03 Release 00

V.1.02 Release 00 -> V.1.03 Release 00 --
Jun. 1, 2007 A Note on Using Debugger Products for the M16C and 740 Families of MCUs (1) With the Tooltip Watch function Fixed
Apr. 16, 2007 A Note on Using the Debuggers for the M16C Family;
the H8/300H Tiny Series, H8 Family; and the 740 Family of MCUs
(1) With loading target programs on MCUs Fixed
Dec. 16, 2006 A Note on Using the Debuggers for the M32C MCU Series (1) With referencing values of IO register in the IO window Fixed
Dec. 16, 2006 A Note on Using Debuggers for the SuperH RISC engine, M16C, H8SX, H8S, H8, and 740 MCU Families (1) With updating debuggers using the AutoUpdate Utility Fixed
Sep. 16, 2006 A Note on Updating the M32C Simulator Debugger On updating the M32C
simulator debugger from V.1.00.00 to V.1.02.00 using the AutoUpdate
utility.
Fixed
Sep. 16, 2006

The Debuggers for the M32C/90, M32C/80, M16C/80, and M16C/70 MCU Series Revised to Their V.1.02 Release 00

V.1.02 Release 00 --


I/O DLL Kit
See Product Information

Issue Date Title Description Status on the
Latest Version
Sep. 1, 2007

Simulator Debugger Customizing Kit I/O DLL Kit V.2.00 Released

Simulator Debugger Customizing Kit I/O DLL Kit V.2.00 is released. --



End of content

Back To Top