|
|
 |
MESC TOOL NEWS:
MESCT-MM-000301D
Please take note of the following problems in using mask file utility MM for Mitsubishi microcomputers:
-
Versions Concerned
Mask file creating utility
MM V.1.00.00 -- V.2.00.10
-
Problems
- (1) When specifying a machine language file name in MM, do not use "DATA:" since "DATA:" is reserved for future use and at present there are no Mitsubishi MCUs to be specified with "DATA:" at creating mask files.
- (2) Note that only one machine language file can be specified whenever
creating a mask file, except for specific products such as MCUs for
OSD.
|
 |